S32G274a - eMMC boot blocks

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32G274a - eMMC boot blocks

1,920件の閲覧回数
nakrachi
Contributor II

Hello,

I am trying to boot from eMMC boot blocks BOOT0/1 partition (mmcblk0boot0 and mmcblk0boot1)

I loaded fip image at an offset of 0x1000, in both BOOT0/1 and User partitions.

I also updated PARTITION_CONFIG  to set it to boot from BOOT0 or BOOT1 partition, but no matter what I do, it always boots from USER partition.

I am wondering, if it is even possible to select boot partitions for booting ? is it a limitation of the BootROM ?

I've tried to set the boot partition with both Linux and u-boot, but no success so far.

=> mmc partconf 0
EXT_CSD[179], PARTITION_CONFIG:
BOOT_ACK: 0x1
BOOT_PARTITION_ENABLE: 0x1
PARTITION_ACCESS: 0x0

 

0 件の賞賛
返信
3 返答(返信)

1,875件の閲覧回数
nakrachi
Contributor II

Thank you,

is there a workaround for this ? can the BootROM be updated/patched ?

0 件の賞賛
返信

1,860件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Thanks for your feedback. On regards of BootROM, we understand that there is no current patch (nor way to do it), we do apologize.

Please, let us know.

1,890件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi 

Overall, we understand that BootROM doesn’t support booting from boot partition of eMMC. We do apologize.

Please, let us know.

0 件の賞賛
返信