S32G274 SPI clock phase configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G274 SPI clock phase configuration

Jump to solution
1,360 Views
Apopo
Contributor I

Use S32DS3.5 and select Example core à Lpspi_Ip_Transter_S32G274A_M7

image.png

 

The configuration needs to be set to CPOL=0, CPHA=0. Is the following setting correct?image.png

If I want to set CPOL=0, CPHA=1, how do I set it?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,339 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @Apopo 
Thanks for your post.

From my understanding, the settings you have made is actually CPOL=0, CPHA=1.

If you want to set with CPOL=0, CPHA=0, then the following settings for your reference.

chenyin_h_0-1736822615793.png

I hope it will help.

 

BR

Chenyin

 

View solution in original post

0 Kudos
Reply
1 Reply
1,340 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @Apopo 
Thanks for your post.

From my understanding, the settings you have made is actually CPOL=0, CPHA=1.

If you want to set with CPOL=0, CPHA=0, then the following settings for your reference.

chenyin_h_0-1736822615793.png

I hope it will help.

 

BR

Chenyin

 

0 Kudos
Reply