S32G2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32G2

3,097件の閲覧回数
mudi69
Contributor I

Hi NXP

        When I programmed the NORFlash of S32G2 through flashtool, the following screenshot appeared. I don’t know why?

0 件の賞賛
返信
3 返答(返信)

3,063件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Which platform are you using? Have you verified that the UART connection is being done through UART0?

Is this error happening after the algorithm is being uploaded to the platform? Or when it is being returned?

How have you configured your platform for the Flashing of the external NOR Flash?

Please, let us know.

0 件の賞賛
返信

3,046件の閲覧回数
mudi69
Contributor I
Hi NXP
        I am using win10. The problem is that some computers can be programmed, and some computers will have the error in the above picture. We have confirmed that the UART connection is fine. The board we use is S32G-VNP-RDB2. The problem is reported when the algorithm is programmed.
0 件の賞賛
返信

3,035件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Thanks for the information.

What preparations have you done for the ones that do not work? You can also use S32DS v3.4 to flash the image directly to NOR Flash. Have you tried this option?

Please, let us know.

0 件の賞賛
返信