S32G2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G2

3,100 Views
mudi69
Contributor I

Hi NXP

        When I programmed the NORFlash of S32G2 through flashtool, the following screenshot appeared. I don’t know why?

0 Kudos
Reply
3 Replies

3,066 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Which platform are you using? Have you verified that the UART connection is being done through UART0?

Is this error happening after the algorithm is being uploaded to the platform? Or when it is being returned?

How have you configured your platform for the Flashing of the external NOR Flash?

Please, let us know.

0 Kudos
Reply

3,049 Views
mudi69
Contributor I
Hi NXP
        I am using win10. The problem is that some computers can be programmed, and some computers will have the error in the above picture. We have confirmed that the UART connection is fine. The board we use is S32G-VNP-RDB2. The problem is reported when the algorithm is programmed.
0 Kudos
Reply

3,038 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Thanks for the information.

What preparations have you done for the ones that do not work? You can also use S32DS v3.4 to flash the image directly to NOR Flash. Have you tried this option?

Please, let us know.

0 Kudos
Reply