S32G2 - How to enable the GMAC driver ( devnp-dwceqos.so) in QNX ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32G2 - How to enable the GMAC driver ( devnp-dwceqos.so) in QNX ?

2,894 次查看
muthu001
Contributor I

Hi,

We are trying to enable GMAC on the NXP S32G2 RDB2 board, on QNX. However, we are getting the error that the driver (devnp-dwceqos.so) is unable to load.

The command used to attach the driver with qnx network management is "io-pkt-v6-hc -d dwceqos"

Error log in slog2info:

muthu001_0-1669635924393.png

 

The OS version: qnx7.1

BSP: BSP_nxp-s32g-evb_br-710_be-710_SVN941162_JBN31

Please help us to get the solution

 

 

0 项奖励
回复
3 回复数

2,884 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We have reached you personally regarding this inquiry.

Have a great day.

0 项奖励
回复

2,874 次查看
muthu001
Contributor I

Hi Daniel,

Thanks for reaching out to us. We are able to up the GMAC0 port. But, IP address not getting assigned using dhcp. Attached screenshot having commands used (marked in blue) and IP address is not assigned ( marked in red). Is it due to PHY not configured properly ?.

Please suggest.

 

Thanks,

Muthu

0 项奖励
回复

2,866 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

As said before, if the problem is related to QNX, we recommend to reach QNX online services on this regard.

As if the problem is the GMAC, have you tried the BSP provided by NXP? Are you having the same problem of the IP not being assigned with DHCP?

Please, let us know.

0 项奖励
回复