S32G2 - How to enable the GMAC driver ( devnp-dwceqos.so) in QNX ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G2 - How to enable the GMAC driver ( devnp-dwceqos.so) in QNX ?

2,890 Views
muthu001
Contributor I

Hi,

We are trying to enable GMAC on the NXP S32G2 RDB2 board, on QNX. However, we are getting the error that the driver (devnp-dwceqos.so) is unable to load.

The command used to attach the driver with qnx network management is "io-pkt-v6-hc -d dwceqos"

Error log in slog2info:

muthu001_0-1669635924393.png

 

The OS version: qnx7.1

BSP: BSP_nxp-s32g-evb_br-710_be-710_SVN941162_JBN31

Please help us to get the solution

 

 

0 Kudos
Reply
3 Replies

2,880 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We have reached you personally regarding this inquiry.

Have a great day.

0 Kudos
Reply

2,870 Views
muthu001
Contributor I

Hi Daniel,

Thanks for reaching out to us. We are able to up the GMAC0 port. But, IP address not getting assigned using dhcp. Attached screenshot having commands used (marked in blue) and IP address is not assigned ( marked in red). Is it due to PHY not configured properly ?.

Please suggest.

 

Thanks,

Muthu

0 Kudos
Reply

2,862 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

As said before, if the problem is related to QNX, we recommend to reach QNX online services on this regard.

As if the problem is the GMAC, have you tried the BSP provided by NXP? Are you having the same problem of the IP not being assigned with DHCP?

Please, let us know.

0 Kudos
Reply