S32G2 ETHERNET MUXING

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32G2 ETHERNET MUXING

2,250件の閲覧回数
JasonTseng
Contributor I

Hello,

Please check p. 10 from below link

https://www.nxp.com/design/training/understanding-the-s32g2-ethernet-architecture:TIP-UNDERSTANDING-...

Q1: S32G2 525FC BGA supports: Max of 3X RGMII/RMII/MII* interfaces (mux options available for all MACs). There are 4 gmac in S32G2 totally, which one of them cannot be RGMII/RMII/MII* interface? and why?

Q2: there is a statement "Each RGMII additionally supports RMII & MII
(*MII requires additional mux signals in LLCE)". which additional mux signal is needed for MII? and why? 

Thanks

0 件の賞賛
返信
3 返答(返信)

2,157件の閲覧回数
JasonTseng
Contributor I

Is there any update?

0 件の賞賛
返信

2,226件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信

2,210件の閲覧回数
JasonTseng
Contributor I

Hello,

I read the link you provided, but it doesn't provide any help with my two questions.

Please provide more specific answers.

Thanks

0 件の賞賛
返信