S32G2 Bootloader

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G2 Bootloader

1,507 Views
PXH1
Contributor I

Hello

We encountered problems when debugging the boot loader to jump to the APP. After jumping to the APP, there will be a chance of getting stuck in the following figure. Sometimes the app can run normally.

PXH1_0-1721812698312.pngPXH1_0-1721812698312.png

We would like to know the possible reasons for entering this place and the solution.

Thanks

 

0 Kudos
Reply
3 Replies

1,488 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

For the information being provided, we understand that this S32G2 bootloader is not one provided from NXP, is this correct?

Please, let us know.

0 Kudos
Reply

1,480 Views
PXH1
Contributor I

Hi,

Both the Bootloader and the APP are routines provided by NXP. Of course, we modified the Bootloader to remove the SD card and EMM-related functions.

PXH1_0-1721872168832.pngPXH1_0-1721872168832.png

For this we want to know, MCAL_LTB_TRACE_OFF triggers the condition, under what circumstances might the program enter.

PXH1_1-1721872296775.pngPXH1_1-1721872296775.png

Is the app missing a macro definition or something?

Thanks

0 Kudos
Reply

1,473 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Thanks for your feedback. When you say the following:

"Of course, we modified the Bootloader to remove the SD card and EMM-related functions."

Did you do it under the code itself? Overall, we don't see much information on regards of the macro you are requesting, given that we don't see much information on regards of modifying the NXP bootloader.

We do apologize.

Please, let us know.

0 Kudos
Reply