S32G-VNP-RDB3 GMAC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G-VNP-RDB3 GMAC

2,062 Views
dongmin
Contributor II

Hi, I'm doing Frame Preemption with GMAC with the S32G-VNP-RDB3 board, but I succeeded with 1G bps. But I'm going to change it to 10M bps, but I can't, so does the limit have to be 1G bps?

Tags (3)
0 Kudos
Reply
5 Replies

1,971 Views
alejandro_e
NXP TechSupport
NXP TechSupport

Hello @dongmin,

Thanks for reaching out to us. About your question, the preemption configuration is not exclusively for 1G bps.  I was able to quickly modify the Gmac_Ip_InternalLoopback, to use preemption and 10M bps and it worked. Please share the following information so I can help you more:

  • What do you mean when you say you "can't" configure it for 10M bps?
  • Please describe how you are testing both configuration.
  • Please share on which core you are running your application.
  • Please share your RTD and/or BSP version.

 

Thanks.

0 Kudos
Reply

1,966 Views
dongmin
Contributor II

First of all, thank you for your answer. I had two S32G-VNP-RDB3 boards and connected GMAC to each other on a 1:1 link, and then proceeded with frame preemption. Core proceeded with M core. I proceeded without using loopback. At this time, I set the clock and settings like a picture, but I saw a phenomenon where the handshake for frame preemption did not occur at this time, just like tx,rx. I need a solution!

dongmin_0-1777943261707.pngdongmin_1-1777943313962.png

 

0 Kudos
Reply

1,612 Views
alejandro_e
NXP TechSupport
NXP TechSupport

hello @dongmin,

Thanks for the details. I will try to reproduce the issue on my side and then find a solution.

If possible please share the information I requested on my last reply.

 

Thanks. 

0 Kudos
Reply

1,596 Views
dongmin
Contributor II

dongmin_0-1778029928224.png

I'm using it like this right now!

0 Kudos
Reply

1,188 Views
alejandro_e
NXP TechSupport
NXP TechSupport

Hello @dongmin,

Sorry for the late reply. I have not been able to reproduce your issue, is it possible to share your project with me? or a stripped version where you can see the problem? You can use the private message functionality of this community or create a private support ticket mentioning this thread.

 

Thanks. 

0 Kudos
Reply