S32G-VNP-RDB2 Missing SJA1110 interfaces in linux BSP 33.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32G-VNP-RDB2 Missing SJA1110 interfaces in linux BSP 33.0

1,618件の閲覧回数
nicolasespla93
Contributor II

Hi!

I'm taking a look to  LNX PFE Driver User Manual  R.T.M 1.1.0  section 4.3.1 to setup the SJA1110 interfaces for the S32G-VNP-RDB2 board. When I follow the steps mentioned in that section:

ip addr add 192.198.100.1 dev pfe0

ip link set pfe0 up

Then, I execute ip addr show, the command only shows pfe0 as available interface but no the other three (enet_pX@pefx  as shown in the attached picture), do I need to make any other configuration to have the other three interfaces as available?

 

My PFE firmware is 1.3, PFE driver 1.0, sja1110_switch.bin and sja1110_uc.bin (from gold vip 1.5).

 

nicolasespla93_0-1676397486301.png

Best regards

Nico

0 件の賞賛
返信
2 返答(返信)

1,593件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We recommend creating a ticket inside NXP online service for this kind of inquiries, since possible debugging is needed.

Please, let us know.

0 件の賞賛
返信

765件の閲覧回数
Armin1
Contributor I
What was the solution to this problem? It would be nice to have it in the driver. Not working around it with vlans for the interface to the users.
0 件の賞賛
返信