S32G LLCE CAN TX

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G LLCE CAN TX

Jump to solution
3,824 Views
longfeiwang
Contributor III

I use the demo "S32G_LLCE_1.0.2->llce_sample_app_pfe" and Bridge Can0 and Can1 busses on S32GRV-PLATEVB. The project can be compiled normally.However, the code is always waiting for the transmission completion of llce can.

"while(txConfirmationCount < (4 * frame_ctr)) ; /* Wait for TX to avoid overloading the TX buffer */"

0 Kudos
Reply
1 Solution
3,812 Views
bpe
NXP Employee
NXP Employee

The Applications team have addressed this issue in the internal training Forum. Please avoid making duplicate posts.

 

Best Regards,
Platon

 

View solution in original post

0 Kudos
Reply
3 Replies
2,617 Views
shanlan123
Contributor II
How do you solve this problem?
0 Kudos
Reply
3,813 Views
bpe
NXP Employee
NXP Employee

The Applications team have addressed this issue in the internal training Forum. Please avoid making duplicate posts.

 

Best Regards,
Platon

 

0 Kudos
Reply
2,616 Views
shanlan123
Contributor II
Where can I see the solution? I still have this problem
0 Kudos
Reply