S32G LLCE CAN TX

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,826件の閲覧回数
longfeiwang
Contributor III

I use the demo "S32G_LLCE_1.0.2->llce_sample_app_pfe" and Bridge Can0 and Can1 busses on S32GRV-PLATEVB. The project can be compiled normally.However, the code is always waiting for the transmission completion of llce can.

"while(txConfirmationCount < (4 * frame_ctr)) ; /* Wait for TX to avoid overloading the TX buffer */"

0 件の賞賛
返信
1 解決策
3,814件の閲覧回数
bpe
NXP Employee
NXP Employee

The Applications team have addressed this issue in the internal training Forum. Please avoid making duplicate posts.

 

Best Regards,
Platon

 

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,619件の閲覧回数
shanlan123
Contributor II
How do you solve this problem?
0 件の賞賛
返信
3,815件の閲覧回数
bpe
NXP Employee
NXP Employee

The Applications team have addressed this issue in the internal training Forum. Please avoid making duplicate posts.

 

Best Regards,
Platon

 

0 件の賞賛
返信
2,618件の閲覧回数
shanlan123
Contributor II
Where can I see the solution? I still have this problem
0 件の賞賛
返信