S32G GMAC not support 802.1AS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32G GMAC not support 802.1AS

3,260件の閲覧回数
AutocoreJin
Contributor I

Hi experts,

 

I noticed that S32G GMAC support 802.1AS. But when I tried to test gPTP on S32G GMAC, it failed.

The reason is that the timestamp got from the network card does not change. As you can see from the figure below:

AutocoreJin_0-1702531099781.png

Use my tool get PTP timestamp from GMAC network card every 5 seconds, but the getting timestamp does not change.

 

The Kernal Version is 

AutocoreJin_1-1702531142895.png

And the PTP option is opened。

AutocoreJin_4-1702531493648.png

 

Is there anything I forgot to do which is necessary for 802.1AS? How can gPTP work correct on S32G GMAC?

Thanks,

Jin

0 件の賞賛
返信
5 返答(返信)

3,054件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @AutocoreJin

We feel very sorry for the delay.

Seems the GMAC PTP is unfunctional, I have the following two suggestions for the issue:

  1. You could try the BSP39, there may be no issues on this version.
  2. If still using the old BSP, may reference the attached workaround patch.

Let me know if it helps.

0 件の賞賛
返信

2,771件の閲覧回数
killedByBugs
Contributor III
Hi Chenyin,

Can you please share the link of the BSP39? I can only see BSP38 on the "automotive software package manager".
Thank you in advance.

Kind Regards,
Jim
0 件の賞賛
返信

3,225件の閲覧回数
nxf92355
NXP Employee
NXP Employee

Hi zhengxiang jin

 

Hope you re doing well

 
you can get information for PTP Support is mentioned under BSP User Manual section. you did't mentioned bsp version that you are using.
I.e bsp 38 -> information for is mentioned under bsp User Manual section 8.
 
 
Best Regards,
Tushar

0 件の賞賛
返信

3,203件の閲覧回数
AutocoreJin
Contributor I

Hi Tushar,

 

Thank you for your response!

My using BSP version is 36.

AutocoreJin_0-1702883906367.png

 

And I read the S32G2_LinuxBSP_36.0_User_Manual 1.pdf. I use ptp4l and try to do time sync but it still does not work.

AutocoreJin_1-1702884009502.png

As you can see, the offset is so huge and do not become smaller.

Do you have any idea about this problem

 

Best Regards,
Jin

 

0 件の賞賛
返信

3,184件の閲覧回数
nxf92355
NXP Employee
NXP Employee

Hi zhengxiang jin

 

Okay , I will regenerate issue and will update.

 

Best Regards ,

Tushar

 

タグ(1)
0 件の賞賛
返信