S32G Cortex M7 Programming / Flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G Cortex M7 Programming / Flash

Jump to solution
8,161 Views
arun_belamge
Contributor III

Hello All.

I have been able to successfully build and generate the IVT blob for the RGB / UART example projects in the S32G DS 3.6. 

Since I currently do not have any Debugger, the only way for me to run the program is via flashing the binary using the Flash Tool.

I have tried many programs and flashed it successfully, but nothing seems to work.

Can anyone tell me where am I going wrong?

For reference,

Main Program:

arun_belamge_2-1760086058368.png

 

Linker:

arun_belamge_1-1760086017588.png

 

IVT Config:

arun_belamge_0-1760085965483.png

Flashing done on QSPI Flash memory as well as SD Card, both load the program successfully but I don't see the LEDs light up or UART print (Linflexd_Uart Example).

Thank you!

0 Kudos
Reply
1 Solution
7,980 Views
Joey_z
NXP Employee
NXP Employee

hi,Contributor II

1.You can try to the baremetal/MCAL RTD demo using this way. 

2. You need to download the package(Integration_Reference_Examples_S32G3_2023_02) to find the file of QSPI configuration. The file foder is the (

C:\nxp\Integration_Reference_Examples_S32G3_2023_02\code\framework\realtime\swc\bootloader\platforms\S32G3XX\res\flash), you can find it in this folder.

Also, I cannot share the project with you, due to the policy of company, sorry for the inconvenience.

BR

Joey

 

View solution in original post

0 Kudos
Reply
20 Replies
8,142 Views
Joey_z
NXP Employee
NXP Employee

hi,

Thank you contacting us.

What is your value of intc_vector? Make sure it is right to be set.

1. You can try to refer to this link for your issue. (https://community.nxp.com/pwmxy87654/attachments/pwmxy87654/S32G/7641/1/S32G-VNP-RDB2-SW-UG.pdf)

2.Also, make sure your project configuration correct, and please try to reduce the size of binary.

Hope this can help you.

BR

Joey

0 Kudos
Reply
8,134 Views
arun_belamge
Contributor III

Hi.

Thank you for the response.

I think i have the intc_vector value correct, please have a look.

arun_belamge_0-1760095705851.png

And I am not sure why the size is a lot more than the one given in the Enablement guide. Can you tell me what could be the reason?

Thank you!

 

0 Kudos
Reply
8,124 Views
Joey_z
NXP Employee
NXP Employee

hi,arun_belamge

Thank you for your reply.

Please modify the linker file , you can try to reduce the size of binary.

BR

Joey

0 Kudos
Reply
8,024 Views
arun_belamge
Contributor III

Hello Joey.

I made minor size changes in linker file and got the size of the binary reduced to less than 3mb, yet the program doesn't work. 

Please help!!!

arun_belamge_1-1760410814305.png

 

arun_belamge_0-1760410781339.png

Thank you.

BR

Arun

0 Kudos
Reply
8,016 Views
Joey_z
NXP Employee
NXP Employee

hi,arun_belamge

Thank you for your reply.

Do you cannot use the demo of uart on  both SD and Qspi mode?

What is your RTD/IDE version?

BR

Joey

0 Kudos
Reply
8,012 Views
arun_belamge
Contributor III
Hi.
Yes I have tried in both SD and QSPI flash, and neither work.
IDE : S32DS 3.6.0
RTD : S32_RTD_5_0_0_QLP03_D2505_ASR_REL_4_4_REV_0000_20250530
Thank you.
BR
Arun
0 Kudos
Reply
7,989 Views
Joey_z
NXP Employee
NXP Employee

hi,arun_belamge

Thank you for your reply.

I have helped you to test the demo of Uart_Example_S32G399A_M7 in RTD 5.0.0, and apply it to use the QSPI mode on RDB3 board. It is the process as the below.

1.Built the demo of Uart and create the .bin file in S32DS IDE. I do not modify any more, just Update Code and Built it.

2. Create the Blob.bin file. You can refer to the configuration as the following picture. 

Joey_z_0-1760426249959.png

3.Flash the blob.bin to Nor Flash and setting the hardware boot from QSPI, then open serial console to choose 9600 baterate, you can find the output information.

Joey_z_1-1760426553231.png

Hope this can help you.

BR

Joey

 

 

0 Kudos
Reply
7,985 Views
arun_belamge
Contributor III
Hi Joey.
Thanks for the support.
I have two questions:
1. Is this example using MCAL or Baremetal? I want to try baremetal.
2. Where can I find the QSPI configuration file?

Also is it possible for you to archive your project as is and attach here, so that i can try to run it without changing anything for testing.

Thank you!

BR
Arun
0 Kudos
Reply
7,981 Views
Joey_z
NXP Employee
NXP Employee

hi,Contributor II

1.You can try to the baremetal/MCAL RTD demo using this way. 

2. You need to download the package(Integration_Reference_Examples_S32G3_2023_02) to find the file of QSPI configuration. The file foder is the (

C:\nxp\Integration_Reference_Examples_S32G3_2023_02\code\framework\realtime\swc\bootloader\platforms\S32G3XX\res\flash), you can find it in this folder.

Also, I cannot share the project with you, due to the policy of company, sorry for the inconvenience.

BR

Joey

 

0 Kudos
Reply
7,975 Views
arun_belamge
Contributor III
Hi Joey.
Tried this and yet after successful flash, I see no output on the UART console.
Is there anyway to know if bootloader is working but application throwing error, or vice-versa.
Should I expect any logs when bootloader fires up?
I am not sure how to debug this...

Thank you for the continued support.

BR
Arun
0 Kudos
Reply
7,954 Views
Joey_z
NXP Employee
NXP Employee

hi,arun_belamge

Could you share your IVT configuration?

This is my S32 Flash Tool configuration, you can try to compare it, make sure your blob.bin flash successfully.

Joey_z_0-1760436141100.png

BR

Joey

0 Kudos
Reply
7,947 Views
arun_belamge
Contributor III

Hi Joey.

Here is the IVT config screenshot:

arun_belamge_2-1760436597540.png

 

Flashing screenshot:

arun_belamge_0-1760436544059.png

Thanks!

 

 

0 Kudos
Reply
7,940 Views
Joey_z
NXP Employee
NXP Employee

hi,arun_belamge

Do you use the customer board or RDB3?

BR

Joey

0 Kudos
Reply
7,937 Views
arun_belamge
Contributor III
Hi Joey.
It's the S32G-VNP-RDB3.

BR
Arun
0 Kudos
Reply
7,887 Views
Joey_z
NXP Employee
NXP Employee

hi,arun_belamge

Could you try to the demo of Uart_Example_S32G399A_M7 in RTD? And refer to my configuration.

BR

Joey

0 Kudos
Reply
7,854 Views
arun_belamge
Contributor III
Hi Joey.
I tried the Uart_Example_S32G399A_M7 with the same configurations as yours, still nothing on the console after flashing.

FYI, I am able to boot Linux BSP through SD card on the A53 core.

BR
Arun
0 Kudos
Reply
7,842 Views
arun_belamge
Contributor III

UPDATE

I reinstalled the S32DS 3.6 and the drivers and now I am able to run the UART Example projects.

But the LED project still doesn't work, this is my code:

arun_belamge_0-1760521119221.png

Please have a look.

Thank you.

BR

Arun

 

0 Kudos
Reply
7,838 Views
Joey_z
NXP Employee
NXP Employee

hi,arun_belamge

Thank you for your reply.

It is good news.

Do you have set the SW11 ON?

Do you have the Multimeter to test the pin?

BR

Joey

0 Kudos
Reply
7,687 Views
arun_belamge
Contributor III
Hi Joey.
Firstly, thank you for the continued support, highly appreciated.
LED i was simply trying to check if M7 boots and works, but since the UART example is working, I have no need for the LED example (anyways, i ll try your suggestion and see the continuity using a multimeter).
For my application I have few doubts, I think for that I will create a new thread.

Thank you.

BR
Arun
0 Kudos
Reply
7,683 Views
Joey_z
NXP Employee
NXP Employee

hi,arun_belamge

Glad to support you.

You can post new ticket if you have any question.

BR

Joey

0 Kudos
Reply