S32G A core reads and writes SRAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G A core reads and writes SRAM

1,196 Views
learnx
Contributor III

Hardware version: S32G274A EVB
Software BSP version: BSP33.0
Software firmware (use official image):
1. binaries_bsp33.0/s32g274ardb2/fsl-image-auto-s32g274ardb2.sdcard 2. binaries_bsp33.0/s32g274ardb2/fip.s32-sdcard
Debugger: Lauterbach
Startup method: SD card startup

Question: Start the A core from the SD card, stay in uboot, use Lauterbach to attach the A core, check the 0x34000000 memory, and display ????. Another phenomenon is that when using the command md.b 0x34000000 0x1000 under uboot, it will crash and then automatically reset.

learnx_0-1706327401780.png

 

0 Kudos
Reply
3 Replies

1,095 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We understand that you are using an EVB platform but see that you are using an RDB2 image, can you confirm that the behavior remains the same by using the EVB related image?

Also, on regards of the "when using the command md.b 0x34000000 0x1000 under uboot, it will crash and then automatically reset." comment, this seems to be related to the memory not being initialized, we can run the command after writing to the related address:

DanielAguirre_0-1706551190916.png

As for the second behavior you are showing, we are unable to reproduce your outcome due to the lack of tools from our side. Still, we see the following from our side:

DanielAguirre_1-1706551458137.png

Don't know if this information helps.

Please, let us know.

0 Kudos
Reply

1,108 Views
learnx
Contributor III

Can anyone help answer this question?

0 Kudos
Reply

1,144 Views
learnx
Contributor III

mw.b mw.w mw.l cannot be cleared ???, mw.q and cp can be cleared

learnx_1-1706353021629.pnglearnx_2-1706353030082.png

 

0 Kudos
Reply