编译好的uboot无法烧写进板子

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

编译好的uboot无法烧写进板子

1,016 Views
yongyang
Contributor I

我修改了uboot但是使用uuu无法烧写进板子。报错如下图所示

yongyang_0-1706577646402.png

 

0 Kudos
Reply
3 Replies

996 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @yongyang

Thanks for the reply.

Well, I am not acting as the i.MX support role, you may try the link below:

https://community.nxp.com/t5/i-MX-Processors/bd-p/imx-processors

Then you may raise a new ticket on the correct forum, there should be i.MX engineers who could provide help.

 

Best Regards

Chenyin

0 Kudos
Reply

1,000 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @yongyang

Thanks for the question.

May I know what kind of board you are working with? S32G2 or S32G3? EVB or RDB?

As far as I know, the UUU is NXP I.MX Chip image deploy tools, it usually is used on i.MX platforms, not targeting for the S32G series, may I know if you could provide more information on your setup?

You may reference the chapter 4 of BSP user manual for writing built images on different booting method if using S32G reference boards.

Let me know if it helps.

 

Best Regards

Chenyin

0 Kudos
Reply

998 Views
yongyang
Contributor I

在你们的哪个网页,突然找不到i.mx系列的了,所以只能是随便选一个系列的了,我的是i.mx系列的。

0 Kudos
Reply