S32DS flash programming with Script language

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32DS flash programming with Script language

1,117件の閲覧回数
Fergani
Contributor II

Hi,

We want to automatize a process with scripting languages, not by opening S32DS, but with a .bat file or something similar. However, we don't know where to start. The thing is that we wrote a code that programs OTP once executing in RAM mode. The second stage will be programming the flash with a xxx.bin file.

How can we achieve this? Can we use tcl scripting or Is there any other way?

 

Best regards

 

 

0 件の賞賛
返信
1 返信

1,101件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

For the available information, this does not seem to be a flow that NXP has documentation on, the expectation is the usage of either S32DS IDE or a different Configuration tool. We see the following HOWTO is available under the S32DS community:

HOWTO: S32 Design Studio Command Line Interface - NXP Community

In which it is shown that under the "Help > Help Contents":

DanielAguirre_0-1712068434708.png

CLI information will be provided.

Aside from this, not much more is provided. We do apologize.

Please, let us know.

0 件の賞賛
返信