S32DS-Import existing project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS-Import existing project

4,634 Views
MohamedAbdelslam
Contributor III

Hi experts, 
I am using S32DS for development and building applications on s32g399ardb3. Normal scenario I am creating workspace an create a project, build , run then push to remote repo. but later i am cloning the repo need to import the project in another workspace but when I am importing or open project it shows me the project as a files not as a project, so Is there any guide or reference for this importing or opening an existing project? I checked the guide but did not get a useful thing 

Tags (1)
0 Kudos
Reply
5 Replies

3,778 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @MohamedAbdelslam 

Thanks for your reply.

Once added, it could be found from the window:

chenyin_h_0-1732845081003.png

Then you may try installing it, once installed, you may need to reset the S32DS to check the latest version.

chenyin_h_1-1732845348190.png

 

BR

Chenyin

0 Kudos
Reply

4,585 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @MohamedAbdelslam 

Thanks for your reply.

I suggest using the S32DS 3.5.3, since it is compatible with most of the examples released.

Temporally I do not have 3.5.0 installed, but we tested it from another host with 3.5.14 and do not find such issue.

Would you mind testing it from 3.5.3?

Thanks.

 

BR

Chenyin

0 Kudos
Reply

4,368 Views
MohamedAbdelslam
Contributor III

Hello, @chenyin_h 
I've downloaded SW32_S32DS_3.5.3_D2306.zip, and it mentioned in the readme file that it is updatesite, so i added it in the s32ds extensions and updates but didn't appear to install it? 
Could you provide how to install it?

Tags (1)
0 Kudos
Reply

4,615 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @MohamedAbdelslam

Thanks for your post.

I have tried it on my S32DS3.5.3. the existing project could be loaded correctly like the following:

chenyin_h_0-1729757820221.png

May I know more details from your operation procedure?

 

BR

Chenyin

0 Kudos
Reply

4,601 Views
MohamedAbdelslam
Contributor III

Hi @chenyin, thank you for reply
First I am using S32DS 3.5 not 3.5.3. when i click on Open Projects from File system and choose my project I find the project as a files not a project as shown in the attached screenshot as i cannot build project until i edit the settings of the project manually by myself (project nature in the setting and add c nature ) and other settings then i can build the project. 

Tags (1)
0 Kudos
Reply