S32DS 3.5 error for Can_Llce_DS_Can2Can_S32G274A_M7 example

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32DS 3.5 error for Can_Llce_DS_Can2Can_S32G274A_M7 example

跳至解决方案
2,787 次查看
salimmulla2021
Contributor III

 

Hello,

I am getting the attached here while opening the Can_Llce_DS_Can2Can_S32G274A_M7  project inside S32DS 3.5. Is it possible to share the version of S32DS supported for this project?

I am using RTD 4.0.0 and LLCE 1.5.0. 

 

 

 

标记 (1)
0 项奖励
回复
1 解答
2,769 次查看
nxf92355
NXP Employee
NXP Employee

Hi Salim Mulla

Hope you are doing well.

Yes, S32DS 3.5 supports example Can_Llce_DS_Can2Can_S32G274A_M7.  Read Document Number: AN13423 (Using CAN2CAN, CAN2ETH and ETH2CAN Features of LLCE on S32G)  which describes install and setup for example . read from chapter 5. i have attached AN13423 please refer.

 

Thanks & Regards ,

Tushar

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,770 次查看
nxf92355
NXP Employee
NXP Employee

Hi Salim Mulla

Hope you are doing well.

Yes, S32DS 3.5 supports example Can_Llce_DS_Can2Can_S32G274A_M7.  Read Document Number: AN13423 (Using CAN2CAN, CAN2ETH and ETH2CAN Features of LLCE on S32G)  which describes install and setup for example . read from chapter 5. i have attached AN13423 please refer.

 

Thanks & Regards ,

Tushar

0 项奖励
回复