Hello,
I am getting the attached here while opening the Can_Llce_DS_Can2Can_S32G274A_M7 project inside S32DS 3.5. Is it possible to share the version of S32DS supported for this project?
I am using RTD 4.0.0 and LLCE 1.5.0.
Solved! Go to Solution.
Hi Salim Mulla
Hope you are doing well.
Yes, S32DS 3.5 supports example Can_Llce_DS_Can2Can_S32G274A_M7. Read Document Number: AN13423 (Using CAN2CAN, CAN2ETH and ETH2CAN Features of LLCE on S32G) which describes install and setup for example . read from chapter 5. i have attached AN13423 please refer.
Thanks & Regards ,
Tushar
Hi Salim Mulla
Hope you are doing well.
Yes, S32DS 3.5 supports example Can_Llce_DS_Can2Can_S32G274A_M7. Read Document Number: AN13423 (Using CAN2CAN, CAN2ETH and ETH2CAN Features of LLCE on S32G) which describes install and setup for example . read from chapter 5. i have attached AN13423 please refer.
Thanks & Regards ,
Tushar