S32 SPI5 could not read data from slave

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 SPI5 could not read data from slave

1,085件の閲覧回数
zhaopingyang_sg
Contributor III

I am trying get data from SPI slave with SPI5

1、Slave device is PCS21125

2、CS is high active,Set PCSIS Bit0 to 1)

3、follow is MISO and clk ,but in Linux driver,read POPR return 0.新建文件4.png

I want to know is anything speical need to when PCSIS Bit is set to 1。 thanks。。。。

0 件の賞賛
返信
1 返信

1,062件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello zhaopingyang,

 

Is the QSPI connected, then its problem of PCS2115, because it is running ok.

 

Regards

0 件の賞賛
返信