S32 SPI5 could not read data from slave

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 SPI5 could not read data from slave

1,081 Views
zhaopingyang_sg
Contributor III

I am trying get data from SPI slave with SPI5

1、Slave device is PCS21125

2、CS is high active,Set PCSIS Bit0 to 1)

3、follow is MISO and clk ,but in Linux driver,read POPR return 0.新建文件4.png

I want to know is anything speical need to when PCSIS Bit is set to 1。 thanks。。。。

0 Kudos
Reply
1 Reply

1,058 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello zhaopingyang,

 

Is the QSPI connected, then its problem of PCS2115, because it is running ok.

 

Regards

0 Kudos
Reply