S32 Design Studio - How to set FreeRTOS cpu clock

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32 Design Studio - How to set FreeRTOS cpu clock

跳至解决方案
2,898 次查看
Boniface
Contributor II

Hello and Happy new year!

I am developing sw for the S32G399A MCU (M7 core) using the S32 Design Studio tool.

My role is to develop the TCP/IP part so I created the example project (lwip_FreeRTOS_S32G399A_M7) and checked it.

After checking, I created a new project and following the contents of the example project.

But the cpu clock[Hz] in the FreeRTOS configuration didn't change even though I followed the exact same settings. (Pins / Clocks / Etc...)

And In the example, the config mode is Default Clock (not the User Clock)

I wannted to upload the screenshot buf unfortunately, due to my company policy, file/screenshot uploads are not allowed.

Could you please how to change the cpu clock?

Thank you.

标记 (1)
0 项奖励
回复
1 解答
2,647 次查看
Joey_z
NXP Employee
NXP Employee

hi,Boniface

Thank you for your reply.

I have the same problem when I use your .mex file, but I did not encounter the problem when I created a new project to add FreeRTOS.I use the 4.0.2 HF3 version of RTD.

Refer to the Release Note, you can try the 4.0.2 version of RTD in S32DS.

Joey_z_0-1737111736999.png

 

BR

Joey

在原帖中查看解决方案

0 项奖励
回复
11 回复数
2,855 次查看
Joey_z
NXP Employee
NXP Employee

Hi,Boniface

Thank you for contacting us.

Which version of RTD and S32DS you are use?

In addition , Are you using a custom board? Is lwip_FreeRTOS_S32G399A_M7 normal for you? How do I get the same version of this routine as yours?

BR

Joey

0 项奖励
回复
2,840 次查看
Boniface
Contributor II

Hi, Joey

Thanks for your reply.

I'm using these SW.

 - S32 Design Studio for S32 Platform V3.5 (Update 14)

 - S32G3 RTD AUTOSAR 4.4 Version 4.0.0

 - FreeRTOS for S32CC 4.0.2

 - TCPIP_STACK for S32G version 1.0.4

 

I got the example by

 : File - New - S32DS Project from Example - S32G TCPIP STACK 1.0.4 D2310 Example Projects - S32G399A - lwip_FreeRTOS_S32G399A_M7

 

And the Target board is S32G-VNP-RDB3.

(Actually, I ordered that board and haven't received it yet.)

 

Best regards,

标记 (1)
0 项奖励
回复
2,824 次查看
Joey_z
NXP Employee
NXP Employee

Hi,Boniface

Thank you for your detailed reply.

You need to fix XBAR_CLK as the following picture.

Joey_z_0-1736755555974.pngJoey_z_1-1736755565791.png

Hope it can help you.

BR

Joey

0 项奖励
回复
2,802 次查看
Boniface
Contributor II

Hi, Joey

 

Unfortunately, I already set XBAR_CLK to 400MHz but it didn't work.

So I attached the MEX file of the project that I create.

I hope this helps you analyze it.

 

Best regards,

Boniface

标记 (1)
0 项奖励
回复
2,778 次查看
Joey_z
NXP Employee
NXP Employee

hi,Boniface

In the FreeRTOS configuration, the CPU clock and XBAR_CLK should maintain the same value. To change the XBAR_CLK, you need to adjust CORE_PLL_DFS1 as shown in the following picture.

Joey_z_0-1736820378619.png

BR

Joey

0 项奖励
回复
2,774 次查看
Boniface
Contributor II

Hi, Joey

Thanks for your fast reply.

I changed the setting but the clock didn't change.

Even though I clicked the Update Code button, deleted and re-added the freertos component in the Peripherals it didn't change.

What else should I check?

Boniface_0-1736821579215.png

Best regards,

Boniface

 

 

标记 (1)
0 项奖励
回复
2,763 次查看
Joey_z
NXP Employee
NXP Employee

hi,Boniface

Thank you for your reply.

I encountered the same problem when testing the provided .mex file.

However, I did not experience the issue when I set up a new project and added FreeRTOS as shown in the following picture. You can try setting up a new project only to add FreeRTOS; then, if the problem still occurs, you could try using version S32DS 3.5.3, which I normally use.

Joey_z_0-1736834694032.png

Joey_z_1-1736834704210.png

Hope it can help you.

BR

Joey

 

0 项奖励
回复
2,674 次查看
Boniface
Contributor II

Hi, Joey

Thank you for your reply.

 

My coworker installed S32DS 3.5.3 and created a new project.

He just added the freertos component after creating the project and the Default clock is still '0'.

(He didn't change the default setting, including clocks.)

Could you please check the mex file I attached?

 

Best regards,

Boniface

 

标记 (1)
0 项奖励
回复
2,648 次查看
Joey_z
NXP Employee
NXP Employee

hi,Boniface

Thank you for your reply.

I have the same problem when I use your .mex file, but I did not encounter the problem when I created a new project to add FreeRTOS.I use the 4.0.2 HF3 version of RTD.

Refer to the Release Note, you can try the 4.0.2 version of RTD in S32DS.

Joey_z_0-1737111736999.png

 

BR

Joey

0 项奖励
回复
2,593 次查看
Boniface
Contributor II

Hi, Joey

 

Finally, I made it.

I installed S32DS 3.5.3 / FreeRTOS 4.0.3 CD3 / SW32G_RTD_4.4_4.0.2_HF02

and It worked.

Thank you for your help.

Boniface_0-1737336828909.png

 

Best Regards,

Boniface

标记 (1)
0 项奖励
回复
2,585 次查看
Joey_z
NXP Employee
NXP Employee

hi,Boniface

I would be glad to help you.

BR

Joey

0 项奖励
回复
%3CLINGO-SUB%20id%3D%22lingo-sub-2024374%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3ES32%20%E8%AE%BE%E8%AE%A1%E5%B7%A5%E4%BD%9C%E5%AE%A4%20-%20%E5%A6%82%E4%BD%95%E8%AE%BE%E7%BD%AE%20FreeRTOS%20CPU%20%E6%97%B6%E9%92%9F%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-2024374%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3E%E6%82%A8%E5%A5%BD%EF%BC%8C%E6%96%B0%E5%B9%B4%E5%BF%AB%E4%B9%90%EF%BC%81%3C%2FP%3E%3CP%3E%E6%88%91%E6%AD%A3%E5%9C%A8%E4%BD%BF%E7%94%A8%20S32%20Design%20Studio%20%E5%B7%A5%E5%85%B7%E4%B8%BA%20S32G399A%20MCU%EF%BC%88M7%20%E6%A0%B8%E5%BF%83%EF%BC%89%E5%BC%80%E5%8F%91%E8%BD%AF%E4%BB%B6%E3%80%82%3C%2FP%3E%3CP%3E%E6%88%91%E7%9A%84%E8%81%8C%E8%B4%A3%E6%98%AF%E5%BC%80%E5%8F%91%20TCP%2FIP%20%E9%83%A8%E5%88%86%EF%BC%8C%E5%9B%A0%E6%AD%A4%E6%88%91%E5%88%9B%E5%BB%BA%E4%BA%86%E7%A4%BA%E4%BE%8B%E9%A1%B9%E7%9B%AE%EF%BC%88%20%3CSTRONG%3Elwip_FreeRTOS_S32G399A_M7%3C%2FSTRONG%3E%20%EF%BC%89%E5%B9%B6%E5%AF%B9%E5%85%B6%E8%BF%9B%E8%A1%8C%E4%BA%86%E6%A3%80%E6%9F%A5%E3%80%82%3C%2FP%3E%3CP%3E%E6%A3%80%E6%9F%A5%E4%B9%8B%E5%90%8E%EF%BC%8C%E6%88%91%E5%88%9B%E5%BB%BA%E4%BA%86%E4%B8%80%E4%B8%AA%E6%96%B0%E9%A1%B9%E7%9B%AE%E5%B9%B6%E9%81%B5%E5%BE%AA%E7%A4%BA%E4%BE%8B%E9%A1%B9%E7%9B%AE%E7%9A%84%E5%86%85%E5%AE%B9%E3%80%82%3C%2FP%3E%3CP%3E%E4%BD%86%E6%98%AF%EF%BC%8C%E5%8D%B3%E4%BD%BF%E6%88%91%E9%81%B5%E5%BE%AA%E5%AE%8C%E5%85%A8%E7%9B%B8%E5%90%8C%E7%9A%84%E8%AE%BE%E7%BD%AE%EF%BC%8CFreeRTOS%20%E9%85%8D%E7%BD%AE%E4%B8%AD%E7%9A%84%3CSTRONG%3ECPU%20%E6%97%B6%E9%92%9F%20%5BHz%5D%3C%2FSTRONG%3E%E4%B9%9F%E6%B2%A1%E6%9C%89%E6%94%B9%E5%8F%98%E3%80%82%EF%BC%88%E5%88%AB%E9%92%88%2F%E6%97%B6%E9%92%9F%2F%E7%AD%89%E7%AD%89...%EF%BC%89%3C%2FP%3E%3CP%3E%E5%9C%A8%E7%A4%BA%E4%BE%8B%E4%B8%AD%EF%BC%8C%E9%85%8D%E7%BD%AE%E6%A8%A1%E5%BC%8F%E6%98%AF%3CSTRONG%3E%E9%BB%98%E8%AE%A4%E6%97%B6%E9%92%9F%3C%2FSTRONG%3E%EF%BC%88%E4%B8%8D%E6%98%AF%E7%94%A8%E6%88%B7%E6%97%B6%E9%92%9F%EF%BC%89%3C%2FP%3E%3CP%3E%E6%88%91%E6%83%B3%E4%B8%8A%E4%BC%A0%E6%88%AA%E5%9B%BE%EF%BC%8C%E4%BD%86%E4%B8%8D%E5%B9%B8%E7%9A%84%E6%98%AF%EF%BC%8C%E7%94%B1%E4%BA%8E%E5%85%AC%E5%8F%B8%E6%94%BF%E7%AD%96%EF%BC%8C%E4%B8%8D%E5%85%81%E8%AE%B8%E4%B8%8A%E4%BC%A0%E6%96%87%E4%BB%B6%2F%E6%88%AA%E5%9B%BE%E3%80%82%3C%2FP%3E%3CP%3E%E4%BD%A0%E8%83%BD%E5%91%8A%E8%AF%89%E6%88%91%E5%A6%82%E4%BD%95%E6%9B%B4%E6%94%B9%20CPU%20%E6%97%B6%E9%92%9F%E5%90%97%EF%BC%9F%3C%2FP%3E%3CP%3E%E8%B0%A2%E8%B0%A2%EF%BC%81%3C%2FP%3E%3C%2FLINGO-BODY%3E