S32 Debug Probe issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 Debug Probe issue

2,731件の閲覧回数
nioer
Contributor I

hi, NXP, when I use the S32 Debug Probe to debug S32G274, there is some problems.

check the picture bellow.

connection is ok.

nioer_0-1648547849793.pngnioer_0-1648547849793.png

nioer_1-1648547893387.pngnioer_1-1648547893387.png

nioer_2-1648547914166.pngnioer_2-1648547914166.png

Could you give us some advice on how to use the S32 Debug Probe?

 

0 件の賞賛
返信
2 返答(返信)

2,553件の閲覧回数
PraveenKumar_K
Contributor II

@nioer did this works for u ? 

I am also facing same kind of problem while using the S32 Debug Probe to debug S32R45 EVK.

could anyone suggest me to solve this S32 Probe issue. @nxp

0 件の賞賛
返信

2,649件の閲覧回数
Yi_Liu_Nxa22412
NXP Employee
NXP Employee

When you connect the S32 debug probe, please make sure:

1. PMIC set to debug mode, PMIC VR5510 won't issue reset to S32G. If the PMIC watchdog reset S32G during S32DS connecting to S32DS, it will report failure.

2. S32G at serial boot mode, the M7_0 core stay at serial boot mode.

0 件の賞賛
返信