S32 Debug Probe issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 Debug Probe issue

2,804 Views
nioer
Contributor I

hi, NXP, when I use the S32 Debug Probe to debug S32G274, there is some problems.

check the picture bellow.

connection is ok.

nioer_0-1648547849793.png

nioer_1-1648547893387.png

nioer_2-1648547914166.png

Could you give us some advice on how to use the S32 Debug Probe?

 

0 Kudos
Reply
2 Replies

2,626 Views
PraveenKumar_K
Contributor II

@nioer did this works for u ? 

I am also facing same kind of problem while using the S32 Debug Probe to debug S32R45 EVK.

could anyone suggest me to solve this S32 Probe issue. @nxp

0 Kudos
Reply

2,722 Views
Yi_Liu_Nxa22412
NXP Employee
NXP Employee

When you connect the S32 debug probe, please make sure:

1. PMIC set to debug mode, PMIC VR5510 won't issue reset to S32G. If the PMIC watchdog reset S32G during S32DS connecting to S32DS, it will report failure.

2. S32G at serial boot mode, the M7_0 core stay at serial boot mode.

0 Kudos
Reply