Qdiscs support in Linux on RDB3 hardware

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Qdiscs support in Linux on RDB3 hardware

1,045件の閲覧回数
yellapu_anishkh
Contributor IV

Hi Team,

We are using RDB3, to configure and use TSN using GMAC interface.

  1. Taprio (IEE 801.Qbv) can be configured in GMAC controller on hardware level.
  2. Do we still need Taprio qdisc, to do similar thing on SW.

 

Question is, if 801.Qbv role is done by qdisc in S/W, what is the role of ethernet controller here ?

if both are used what is the work offloaded to SW in comparison to HW ?

タグ(5)
0 件の賞賛
返信
0 返答(返信)