URGENT - PFE and Bridge creation Support

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

URGENT - PFE and Bridge creation Support

1,167 次查看
dramadan
Contributor II

Hello, 

 

Kindly, Bridges creation introduces high CPU load. It takes more than 1 seconds to create three bridges. We are trying to reduce this CPU load issue. We have the following questions: 

1- What is NXP expectation time for PFE bridge creation?
2- Why do we need more than one bridge to comm between A53 and M7?
3- Is the Auxuliry mandatory to communicate between A53 and M7?. If No, what are other options?
4- If more than one bridge is needed, is it possible to have Eth messages after the first one and not wait for all bridge creation?

标记 (1)
0 项奖励
回复
2 回复数

1,119 次查看
Aubineau_FAE
NXP Employee
NXP Employee

It is not normal to take 1 second. Can you describe in detail,  what is the relevant code you did?

0 项奖励
回复

1,088 次查看
Aubineau_FAE
NXP Employee
NXP Employee

Hi Doria,

Any feedback?

0 项奖励
回复