I have downloaded and installed below packages
1. EB tresos AutoCore for S32G3 2. GoldVIP for S32G3
followed the GoldVip manual for applying patch and copying MCAL_ext plugins.
but while importing it to the eb , it is asking to remove multiple plugins as some doesn't exits there .
kindly let me know where i can get the proper plugins supporting GoldVIP , how to proceed without any errors
已解决! 转到解答。
Hello!!!
Finally i am able to import the package
i removed the below mentioned link from EB installation directory EB\tresos\links
Since RTD and llce and macalExt modules are having same plugings i hope these where causing the error
Hello!!!
Finally i am able to import the package
i removed the below mentioned link from EB installation directory EB\tresos\links
Since RTD and llce and macalExt modules are having same plugings i hope these where causing the error
Previously i had done a mistake while installing ,
now i followed, first installed eb then installed 4.0.2 HF02 now i am able to find the previous missing plugins but ended up here with error "Cannot load configuration Dio. Another module already created a configuration at /AUTOSAR/TOP-LEVEL-PACKAGES/Dio/ELEMENTS/Dio " asking me to remove those mcal drivers
Hi,
Was the project deleted from workspace after the plugins were correctly installed? Or is this the same project which was imported at the beginning?
We recommend reimporting the project, since the plugins were not correct and could have caused a misconfiguration.
Please, let us know.
Hi,
Thanks for your feedback. Have you applied the following modifications to the plugins inside EB Tresos?
Where you should delete some plugins and replace others.
Please, let us know.
Yes , I followed these setup, and did these recommended changes after that , I closed the eb and workspace deleted work space and once again importanted package on eb then i got these errors