Not able to load the Goldvip can-gw on eb tresos studio

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Not able to load the Goldvip can-gw on eb tresos studio

Jump to solution
1,175 Views
Karthik_7
Contributor III

Karthik_7_0-1710953481829.png

I have downloaded and installed below packages 
1. EB tresos AutoCore for S32G3      2. GoldVIP for S32G3

followed the GoldVip manual for applying patch and copying MCAL_ext plugins.

but while importing it to the eb , it is asking to remove multiple plugins as some doesn't exits there .

kindly let me know where i can get the proper plugins supporting GoldVIP , how to proceed without any errors   

Labels (1)
0 Kudos
Reply
1 Solution
1,028 Views
Karthik_7
Contributor III

Hello!!!
Finally i am able to import the package 
i removed the below mentioned link from EB installation directory EB\tresos\links

Karthik_7_0-1711081590772.png

Since RTD and llce and macalExt modules are having same plugings i hope these where causing the error

View solution in original post

0 Kudos
Reply
8 Replies
1,029 Views
Karthik_7
Contributor III

Hello!!!
Finally i am able to import the package 
i removed the below mentioned link from EB installation directory EB\tresos\links

Karthik_7_0-1711081590772.png

Since RTD and llce and macalExt modules are having same plugings i hope these where causing the error

0 Kudos
Reply
1,153 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Can you help us share a capture of the message you are seeing?

Please, let us know.

0 Kudos
Reply
1,142 Views
Karthik_7
Contributor III

Karthik_7_0-1711033269712.png

Previously i had done a mistake while installing ,
now i followed, first installed eb then installed 4.0.2 HF02 now i am able to find the previous missing plugins but ended up here with error "Cannot load configuration Dio. Another module already created a configuration at /AUTOSAR/TOP-LEVEL-PACKAGES/Dio/ELEMENTS/Dio " asking me to remove those mcal drivers

0 Kudos
Reply
1,120 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Was the project deleted from workspace after the plugins were correctly installed? Or is this the same project which was imported at the beginning?

We recommend reimporting the project, since the plugins were not correct and could have caused a misconfiguration.

Please, let us know.

0 Kudos
Reply
1,116 Views
Karthik_7
Contributor III

Yes , I deleted it , I had a zip backup so I tried re importing it , but ended up with above error 

0 Kudos
Reply
1,103 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Thanks for your feedback. Have you applied the following modifications to the plugins inside EB Tresos?

DanielAguirre_0-1711052997968.png

Where you should delete some plugins and replace others.

Please, let us know.

0 Kudos
Reply
1,085 Views
Karthik_7
Contributor III

Yes , I followed these setup, and did these recommended changes  after that , I closed the eb and workspace deleted work space and once again importanted package on eb  then i got these errors 

0 Kudos
Reply
1,086 Views
Karthik_7
Contributor III

Yes , I did these recommended changes 

0 Kudos
Reply