Not able to load the Goldvip can-gw on eb tresos studio

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Not able to load the Goldvip can-gw on eb tresos studio

跳至解决方案
1,070 次查看
Karthik_7
Contributor III

Karthik_7_0-1710953481829.png

I have downloaded and installed below packages 
1. EB tresos AutoCore for S32G3      2. GoldVIP for S32G3

followed the GoldVip manual for applying patch and copying MCAL_ext plugins.

but while importing it to the eb , it is asking to remove multiple plugins as some doesn't exits there .

kindly let me know where i can get the proper plugins supporting GoldVIP , how to proceed without any errors   

标签 (1)
0 项奖励
回复
1 解答
923 次查看
Karthik_7
Contributor III

Hello!!!
Finally i am able to import the package 
i removed the below mentioned link from EB installation directory EB\tresos\links

Karthik_7_0-1711081590772.png

Since RTD and llce and macalExt modules are having same plugings i hope these where causing the error

在原帖中查看解决方案

0 项奖励
回复
8 回复数
924 次查看
Karthik_7
Contributor III

Hello!!!
Finally i am able to import the package 
i removed the below mentioned link from EB installation directory EB\tresos\links

Karthik_7_0-1711081590772.png

Since RTD and llce and macalExt modules are having same plugings i hope these where causing the error

0 项奖励
回复
1,048 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Can you help us share a capture of the message you are seeing?

Please, let us know.

0 项奖励
回复
1,037 次查看
Karthik_7
Contributor III

Karthik_7_0-1711033269712.png

Previously i had done a mistake while installing ,
now i followed, first installed eb then installed 4.0.2 HF02 now i am able to find the previous missing plugins but ended up here with error "Cannot load configuration Dio. Another module already created a configuration at /AUTOSAR/TOP-LEVEL-PACKAGES/Dio/ELEMENTS/Dio " asking me to remove those mcal drivers

0 项奖励
回复
1,015 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Was the project deleted from workspace after the plugins were correctly installed? Or is this the same project which was imported at the beginning?

We recommend reimporting the project, since the plugins were not correct and could have caused a misconfiguration.

Please, let us know.

0 项奖励
回复
1,011 次查看
Karthik_7
Contributor III

Yes , I deleted it , I had a zip backup so I tried re importing it , but ended up with above error 

0 项奖励
回复
998 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Thanks for your feedback. Have you applied the following modifications to the plugins inside EB Tresos?

DanielAguirre_0-1711052997968.png

Where you should delete some plugins and replace others.

Please, let us know.

0 项奖励
回复
980 次查看
Karthik_7
Contributor III

Yes , I followed these setup, and did these recommended changes  after that , I closed the eb and workspace deleted work space and once again importanted package on eb  then i got these errors 

0 项奖励
回复
981 次查看
Karthik_7
Contributor III

Yes , I did these recommended changes 

0 项奖励
回复