NXP S32G3 VNP RDB3 Failure to boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP S32G3 VNP RDB3 Failure to boot

2,734 Views
Jayanth-KB
Contributor III

Dear NXP Support Team,

We have recently purchased the S32G3 VNP-RDB3 board and are encountering an issue during the boot process. After flashing BSP Linux 43.0, which was downloaded from the NXP website, the board fails to boot successfully.

The console repeatedly displays the following messages:

NOTICE: Reset status: Power-On Reset
PANIC at PC : 0x000000000000003f DDR subsystem


We would greatly appreciate your assistance in resolving this issue or any guidance you can provide to help us proceed.

Best regards,
Jayanth KB

Tags (1)
0 Kudos
Reply
7 Replies

2,607 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @Jayanth-KB 

Thanks for your reply.

From the information shared, it is possible that there are hardware issues on your board.

I suggest contacting the distributor where you bought the board directly to have a replacement if possible.

If not available, an alternative way is that to request  "Return for Replacement" process from the following link:

https://www.nxp.com/support/sample-and-buy/how-to-buy-from-nxp/dev-tool-warranty-return-request-form...

Apologize for your inconvenience.

 

BR

Chenyin

0 Kudos
Reply

2,628 Views
chenyin_h
NXP Employee
NXP Employee
Hello,  @Jayanth-KB 
Tanks for your reply.
In order for connecting the board with DDR tools:
Firstly, you may have to change the switches on the board to "serial boot mode"; secondly, connect the UART0 to your PC; thirdly, open the S32DS, create or import a S32G3 project, then enter DDR tools, the necessary operation may be similar to: 
chenyin_h_0-1747103773496.png

Click on the "start Validation" to check the DDR.

 

BR

Chenyin

0 Kudos
Reply

2,613 Views
Jayanth-KB
Contributor III

Dear @chenyin_h,

Thanks for your reply.

I will follow the steps you outlined: switching the board to serial boot mode, connecting UART0 to my PC, and then using S32DS to create or import an S32G3 project before accessing the DDR tools.

JayanthKB_0-1747118701103.png

There was a validation failure. Please let me know if there are any specific settings or additional considerations I should be aware of during this process.

Best regards,

Jayanth K B

 

Tags (1)
0 Kudos
Reply

2,672 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @Jayanth-KB 

Thanks for your reply

I suggest doing the following tests:

1. Firstly, to check the 4th option I posted in previous reply, to check if there is still issues.

2. If yes, would you mind connecting your new board with S32DS, and to use the DDR tool to validate the board

 

BR

Chenyin

0 Kudos
Reply

2,655 Views
Jayanth-KB
Contributor III

Dear @chenyin_h,

Thanks for the suggestions.

Regarding point 2, could you please share the detailed steps to connect the new board with S32DS and use the DDR tool to validate it? That would be very helpful.

Looking forward to your guidance.

Best regards,

Jayanth KB

Tags (1)
0 Kudos
Reply

2,724 Views
chenyin_h
NXP Employee
NXP Employee
Hello, @Jayanth-KB 
 
Thanks for your post.
From the log you shared, I have the following suggestions:
1. Not sure if you have other board that could be boot correctly, if yes, use the SD card which could boot other board correctly to test on the board with failure prints. 
2. Change another SD card to try booting the board.
3. Use DDR tool from S32DS to check the DDR status of the board.
4. Occasionally there may be some false contact on the SoC. if pushing it on the board, it may boots correctly.
 
If still issue existed, then the issue may well be caused by hardware issue, you may request a hardware replacement.
Sorry for your inconvenience.  
 
BR
Chenyin
0 Kudos
Reply

2,712 Views
Jayanth-KB
Contributor III

Dear @chenyin_h ,

As a follow-up, I would like to share that we have another S32G3 VNP-RDB3 board that is functioning correctly. To isolate the issue, we tested the same SD card—originally used in the working board—on the new board that is experiencing the boot issue. Unfortunately, the new board still fails to boot, indicating that the problem is likely New Board

We would greatly appreciate your assistance in diagnosing and resolving this issue, or any further guidance you can provide.

Best regards,
Jayanth KB

Tags (1)
0 Kudos
Reply