LLCE_LIN S32G-VNP-RDB2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LLCE_LIN S32G-VNP-RDB2

ソリューションへジャンプ
4,346件の閲覧回数
HuiLing
Contributor II

I want to implement the use of LLCE_LIN, I downloaded the LLCE firmware version 1.07, using the sample:

HuiLing_0-1702955977610.png

But I can't run, compile an error.

The original peripheral configurations are as follows:

HuiLing_1-1702956259755.png

The compilation error is as follows:

HuiLing_2-1702956347029.png

 

Error after adding missing set of header files:

HuiLing_0-1702962731377.png

What are the requirements and configurations for this project?

 

0 件の賞賛
返信
1 解決策
4,270件の閲覧回数
HuiLing
Contributor II
Thank you very much for your help. I have solved it.

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
4,297件の閲覧回数
HuiLing
Contributor II

hi@ Daniel-Aguirre

Due to this error:arm-none-eabi-gcc -o "Lin_Llce_DS_S32G274A_M7_2.elf" "@Lin_Llce_DS_S32G274A_M7_2.args"
e:/nxp/s32ds.3.5/s32ds/build_tools/gcc_v9.2/gcc-9.2-arm32-eabi/bin/../lib/gcc/arm-none-eabi/9.2.0/../../../../arm-none-eabi/bin/real-ld.exe: ./src/Platform_Init.o: in function `PlatformInit':
E:\Users\workspaceS32DS.3.5\Lin_Llce_DS_S32G274A_M7_2\Debug_RAM/../src/Platform_Init.c:50: undefined reference to `Rm_Init'
collect2.exe: error: ld returned 1 exit status
make: *** [makefile:40: Lin_Llce_DS_S32G274A_M7_2.elf] Error 1
"make -j16 all" terminated with exit code 2. Build might be incomplete.

13:40:57 Build Failed. 2 errors, 0 warnings. (took 3s.747ms)

I added RM to the component,

HuiLing_0-1703051925233.png

HuiLing_1-1703051957007.png

Then I can go through the compile, but when debug appears in this place to hang up:

HuiLing_2-1703052043963.png

Do I need to add this RM component? If so, is this component not configured properly? How it should be configured; If not, how to solve the above error?

I hope to get your help, thank you!

Best Regards,HuiLing
 
 
0 件の賞賛
返信
4,277件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Thanks for your feedback. The Rm component seems to be related to XRDC, which is a module dedicated to isolating resources. Since you only added it to the project, it might be that there was no resources configured for the specific domain.

As for compilation, we understand that there might have been some bugs under this specific example. Help us doing the following steps to understand if you are able to compile successfully:

1. Generate the code from Config Tools (no modifications up-to this point)

2. Modify the variable under the Mcu_Init function:

DanielAguirre_0-1703083275517.png

3. Comment all XRDC/Rm includes/functions:

DanielAguirre_1-1703083336921.png

...

DanielAguirre_2-1703083352051.png

4. As per the "description.txt" file under the example, add the required modules and delete the specific source file.

5. Delete the source file "generate/src/Clock_Ip_PBcfg.c"

With that, we are able to compile the example no problem:

DanielAguirre_3-1703083702758.png

Please, let us know.

0 件の賞賛
返信
4,271件の閲覧回数
HuiLing
Contributor II
Thank you very much for your help. I have solved it.
0 件の賞賛
返信
4,319件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

For the last compilation error that you are seeing, it seems that the variant name was not updated correctly under the example. Help us change the function as follows:

DanielAguirre_0-1703012703566.png

Please, let us know.

0 件の賞賛
返信
4,298件の閲覧回数
HuiLing
Contributor II
Hi
Thanks for your help, the following errors have appeared after modification:
arm-none-eabi-gcc -o "Lin_Llce_DS_S32G274A_M7_2.elf" "@Lin_Llce_DS_S32G274A_M7_2.args"
e:/nxp/s32ds.3.5/s32ds/build_tools/gcc_v9.2/gcc-9.2-arm32-eabi/bin/../lib/gcc/arm-none-eabi/9.2.0/../../../../arm-none-eabi/bin/real-ld.exe: ./src/Platform_Init.o: in function `PlatformInit':
E:\Users\workspaceS32DS.3.5\Lin_Llce_DS_S32G274A_M7_2\Debug_RAM/../src/Platform_Init.c:50: undefined reference to `Rm_Init'
collect2.exe: error: ld returned 1 exit status
make: *** [makefile:40: Lin_Llce_DS_S32G274A_M7_2.elf] Error 1
"make -j16 all" terminated with exit code 2. Build might be incomplete.

13:40:57 Build Failed. 2 errors, 0 warnings. (took 3s.747ms)
0 件の賞賛
返信