Issue with NFS Boot on S32G

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Issue with NFS Boot on S32G

417 次查看
ibrahimhabibpn
Contributor I

I followed the instructions in the Linux BSP User Manual under the "Booting from NFS" section. After running the following command:
nfsboot

I encountered the following error in kernel logs

[ TC: R1served shabed memmry:5s enSDled
8/T :iDynamitr[ 1.169519] optee: revision 4.0 (5b73ca90)
[ 1.174443] optee: dynamic shared memory is enabled
[ C:2.076
1/TC:2 c Core data2 bort4
ad7[ 27.049468] rcu: INFO: rcu_preempt detected stalls on CPUs/tasks:
[ 27.055557] rcu: 2-...0: (63 ticks this GP) idle=7a7/1/0x4000000000000000 softirq=44/46 fqs=1333
[ 27.064645] (detected by 0, t=5254 jiffies, g=-1131, q=3)
[ 27.070204] Task dump for CPU 2:
[ 27.073471] task:swapper/0 state:R running task stack: 0 pid: 1 ppid: 0 flags:0x0000000a
[ 27.083527] Call trace:
[ 27.085998] __switch_to+0xf8/0x14c
[ 27.089542] 0xc0
[ 48.149466] rcu: INFO: rcu_preempt detected stalls on CPUs/tasks:
[ 48.155639] rcu: 2-...0: (63 ticks this GP) idle=7a7/1/0x4000000000000000 softirq=44/46 fqs=2681
[ 48.164727] (detected by 0, t=10529 jiffies, g=-1131, q=3)
[ 48.170373] Task dump for CPU 2:
[ 48.173637] task:swapper/0 state:R running task stack: 0 pid: 1 ppid: 0 flags:0x0000000a
[ 48.183691] Call trace:
[ 48.186162] __switch_to+0xf8/0x14c
[ 48.189696] 0xc0
[ 69.253466] rcu: INFO: rcu_preempt detected stalls on CPUs/tasks:
[ 69.259640] rcu: 2-...0: (63 ticks this GP) idle=7a7/1/0x4000000000000000 softirq=44/46 fqs=3887
[ 69.268725] (detected by 0, t=15805 jiffies, g=-1131, q=3)
[ 69.274370] Task dump for CPU 2:
[ 69.277634] task:swapper/0 state:R running task stack: 0 pid: 1 ppid: 0 flags:0x0000000a
[ 69.287685] Call trace:
[ 69.290156] __switch_to+0xf8/0x14c
[ 69.293689] 0xc0
[ 90.345466] rcu: INFO: rcu_preempt detected stalls on CPUs/tasks:
[ 90.351639] rcu: 2-...0: (63 ticks this GP) idle=7a7/1/0x4000000000000000 softirq=44/46 fqs=4961
[ 90.360724] (detected by 0, t=21080 jiffies, g=-1131, q=3)
[ 90.366368] Task dump for CPU 2:
[ 90.369633] task:swapper/0 state:R running task stack: 0 pid: 1 ppid: 0 flags:0x0000000a
[ 90.379684] Call trace:
[ 90.382155] __switch_to+0xf8/0x14c
[ 90.385688] 0xc0
[ 111.417466] rcu: INFO: rcu_preempt detected stalls on CPUs/tasks:
[ 111.423640] rcu: 2-...0: (63 ticks this GP) idle=7a7/1/0x4000000000000000 softirq=44/46 fqs=6301
[ 111.432723] (detected by 0, t=26346 jiffies, g=-1131, q=3)
[ 111.438368] Task dump for CPU 2:
[ 111.441632] task:swapper/0 state:R running task stack: 0 pid: 1 ppid: 0 flags:0x0000000a
[ 111.451683] Call trace:
[ 111.454154] __switch_to+0xf8/0x14c
[ 111.457686] 0xc0
[ 132.505465] rcu: INFO: rcu_preempt detected stalls on CPUs/tasks:
[ 132.511640] rcu: 2-...0: (63 ticks this GP) idle=7a7/1/0x4000000000000000 softirq=44/46 fqs=7713
[ 132.520727] (detected by 0, t=31620 jiffies, g=-1131, q=3)
[ 132.526371] Task dump for CPU 2:
[ 132.529635] task:swapper/0 state:R running task stack: 0 pid: 1 ppid: 0 flags:0x0000000a
[ 132.539686] Call trace:
[ 132.542157] __switch_to+0xf8/0x14c
[ 132.545691] 0xc0
[ 153.569465] rcu: INFO: rcu_preempt detected stalls on CPUs/tasks:
[ 153.575639] rcu: 2-...0: (63 ticks this GP) idle=7a7/1/0x4000000000000000 softirq=44/46 fqs=10345
[ 153.584812] (detected by 0, t=36886 jiffies, g=-1131, q=3)
[ 153.590457] Task dump for CPU 2:
[ 153.593720] task:swapper/0 state:R running task stack: 0 pid: 1 ppid: 0 flags:0x0000000a
[ 153.603772] Call trace:
[ 153.606244] __switch_to+0xf8/0x14c
[ 153.609778] 0xc0
[ 174.633465] rcu: INFO: rcu_preempt detected stalls on CPUs/tasks:
[ 174.639639] rcu: 2-...0: (63 ticks this GP) idle=7a7/1/0x4000000000000000 softirq=44/46 fqs=12977
[ 174.648814] (detected by 0, t=42152 jiffies, g=-1131, q=4)
[ 174.654458] Task dump for CPU 2:
[ 174.657723] task:swapper/0 state:R running task stack: 0 pid: 1 ppid: 0 flags:0x0000000a
[ 174.667775] Call trace:
[ 174.670246] __switch_to+0xf8/0x14c
[ 174.673780] 0xc0
[ 195.697466] rcu: INFO: rcu_preempt detected stalls on CPUs/tasks:
[ 195.703640] rcu: 2-...0: (63 ticks this GP) idle=7a7/1/0x4000000000000000 softirq=44/46 fqs=15609
[ 195.712812] (detected by 0, t=47418 jiffies, g=-1131, q=4)

标记 (3)
0 项奖励
回复
0 回复数