Is there kernel source code available for NXP PMIC drivers?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there kernel source code available for NXP PMIC drivers?

ソリューションへジャンプ
1,442件の閲覧回数
Jeff-CF-Huang
Contributor III

Is there kernel source code available for NXP PMIC drivers, such as PF5020, MPS5600, VR5510, or PF5300?

0 件の賞賛
返信
1 解決策
1,425件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @Jeff-CF-Huang 

Thanks for the post.

There are not such drivers existed in the kernel source from BSP perspective.

 

BR

Chenyin

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,426件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @Jeff-CF-Huang 

Thanks for the post.

There are not such drivers existed in the kernel source from BSP perspective.

 

BR

Chenyin

0 件の賞賛
返信
%3CLINGO-SUB%20id%3D%22lingo-sub-1986750%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3ENXP%20PMIC%E3%83%89%E3%83%A9%E3%82%A4%E3%83%90%E7%94%A8%E3%81%AE%E3%82%AB%E3%83%BC%E3%83%8D%E3%83%AB%E3%82%BD%E3%83%BC%E3%82%B9%E3%82%B3%E3%83%BC%E3%83%89%E3%81%AF%E3%81%82%E3%82%8A%E3%81%BE%E3%81%99%E3%81%8B%3F%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-1986750%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3EPF5020%E3%80%81MPS5600%E3%80%81VR5510%E3%80%81PF5300%20%E3%81%AA%E3%81%A9%E3%81%AE%20NXP%20PMIC%20%E3%83%89%E3%83%A9%E3%82%A4%E3%83%90%E3%83%BC%E7%94%A8%E3%81%AE%E3%82%AB%E3%83%BC%E3%83%8D%E3%83%AB%20%E3%82%BD%E3%83%BC%E3%82%B9%20%E3%82%B3%E3%83%BC%E3%83%89%E3%81%AF%E3%81%82%E3%82%8A%E3%81%BE%E3%81%99%E3%81%8B%3F%3C%2FP%3E%3C%2FLINGO-BODY%3E