Is there kernel source code available for NXP PMIC drivers?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there kernel source code available for NXP PMIC drivers?

Jump to solution
1,438 Views
Jeff-CF-Huang
Contributor III

Is there kernel source code available for NXP PMIC drivers, such as PF5020, MPS5600, VR5510, or PF5300?

0 Kudos
Reply
1 Solution
1,421 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @Jeff-CF-Huang 

Thanks for the post.

There are not such drivers existed in the kernel source from BSP perspective.

 

BR

Chenyin

View solution in original post

0 Kudos
Reply
1 Reply
1,422 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @Jeff-CF-Huang 

Thanks for the post.

There are not such drivers existed in the kernel source from BSP perspective.

 

BR

Chenyin

0 Kudos
Reply