If any examples for S32G2 Multicore use the same project with FreeRTOS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

If any examples for S32G2 Multicore use the same project with FreeRTOS

1,600件の閲覧回数
bakerliu
Contributor I

Hi,

I was wondering if there are any examples of using FreeRTOS with S32G2 multicore M7 processors. Please let me know if the same project can be used for this purpose.

Thanks and regards,
Baker

0 件の賞賛
返信
4 返答(返信)

1,570件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

The main example that is provided for multicore application under the S32G platform is the one explained on the AN13750 available under the S32G2 product page (link: S32G2 Safe and Secure Vehicle Network Processor | NXP Semiconductors).

It can be done integrating FreeRTOS, but there is not an out-of-the-box example that uses FreeRTOS. We do apologize.

Please, let us know.

0 件の賞賛
返信

1,567件の閲覧回数
bakerliu
Contributor I

Hi,

I have created a multicore application using S32DS, but it is separated into three projects. I am wondering if it is possible to create a single project application that runs on the multicore M7 using a single image file?

Thank you.

0 件の賞賛
返信

1,550件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Thanks for your feedback.

Under the S32G platform, the multicore application requires independent files. This means that each core has its own application. Hence, no single file (at this moment) multicore application is possible. That is why AN13750 uses different files for each core.

We apologize for this.

Please, let us know.

0 件の賞賛
返信

1,539件の閲覧回数
bakerliu
Contributor I

Hi,
 
Thank you for your response. I appreciate your prompt attention and assistance. If I have any further questions, I'll be sure to reach out.

Thanks again!

0 件の賞賛
返信