IVT Config Error "Application Boot Code Image not include head file."

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IVT Config Error "Application Boot Code Image not include head file."

2,007 Views
Archieeeee
Contributor II

Hi  expert:

i build the bootaloder image, step by <S32G_Bootloader_V2>

when i make the ivt dcd image , S32DS IVT Config Tool report error "Application Boot Code Image not include head file. the export file must be complete"

 

 

image.png

this issue can  recurrented by 3 step

step 1:

add S32G274_QuadSPI_133MHz_DDR_configuration.bin in Interface selection 

file path :D:\NXP\Integration_Reference_Examples_S32G2_2023_06\code\framework\realtime\swc\bootloader\platforms\S32G2XX\res\flash

image.png

step 2

add S32G274_DCD_InitSRAM.bin in  DCD

image.png

step3:

add Bootloader.bin  in Application bootloader

Archieeeee_0-1706764567980.png

 

Pls Help

0 Kudos
Reply
2 Replies

1,983 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

For the error you are mentioning:

"Application Boot Code Image not include head file. the export file must be complete"

It seems that the Application Bootloader has not been exported, as shown below:

DanielAguirre_1-1706808660292.pngDanielAguirre_2-1706808723173.png

Please, let us know.

 

1,959 Views
Archieeeee
Contributor II

Hi  Daniel:

thanks for you reply,

 it's work ok, after export image