IPCF v4.10 kernel sample driver dependency issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IPCF v4.10 kernel sample driver dependency issue

1,672件の閲覧回数
hittzt
Senior Contributor I

Hi,

 

I noticed that IPCF v4.10 driver has been released for a period of time, and I tried to compile the sample, i.e, ipc-shm-sample.ko and ipc-shm-dev.ko, for native linux. But unfortunatly, compilation failed, the reason is that, the ipc-shm-sample.ko wrongly depends on ipc-shm-xen.ko, as the following line in ipc-shm-sample.mod.c:

MODULE_INFO(depends, "ipc-shm-xen");

and the right dependency should be: MODULE_INFO(depends, "ipc-shm-dev");

So could you please help to check the issue?

 

Thanks,

Zhantao

0 件の賞賛
返信
3 返答(返信)

1,641件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hi, @hittzt 

Thanks for your reply.

Yes, I noticed it from the code

But I tested it on my local RDB3, based on BSP42, I do not see errors/warning prints while testing with IPCF sample

root@s32g399ardb3:~# insmod ipc-shm-dev.ko
root@s32g399ardb3:~# insmod ipc-shm-sample.ko
root@s32g399ardb3:~# lsmod
Module Size Used by
ipc_shm_sample 12288 0
ipc_shm_dev 36864 1 ipc_shm_sample
sja1110 20480 0
root@s32g399ardb3:~# dmesg | tail
[ 8.981273] s32cc-dwmac 4033c000.ethernet eth0: Enabling Safety Features
[ 8.981368] s32cc-dwmac 4033c000.ethernet eth0: IEEE 1588-2008 Advanced Timestamp supported
[ 8.981640] s32cc-dwmac 4033c000.ethernet eth0: registered PTP clock
[ 8.982063] s32cc-dwmac 4033c000.ethernet eth0: FPE workqueue start
[ 8.982075] s32cc-dwmac 4033c000.ethernet eth0: configuring for phy/rgmii-id link mode
[ 8.984809] 8021q: adding VLAN 0 to HW filter on device eth0
[ 11.901187] random: crng init done
[ 13.085991] s32cc-dwmac 4033c000.ethernet: Setting TX clock to 125000000 Hz
[ 13.086069] s32cc-dwmac 4033c000.ethernet eth0: Link is Up - 1Gbps/Full - flow control rx/tx
[ 16.976019] systemd[355]: memfd_create() called without MFD_EXEC or MFD_NOEXEC_SEAL set

So it seems not impact the module loading sequence.

 

BR

Chenyin

0 件の賞賛
返信

1,662件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @hittzt 

Thanks a lot for your post.

I will check it later, I undertand that you were building it manually instead of Yocto, right?

 

BR

Chenyin

 

BR

Chenyin

0 件の賞賛
返信

1,646件の閲覧回数
hittzt
Senior Contributor I

Hi @chenyin_h,

 

To make it clear, it should not say "compilation failed" in my original description, acctually, the compilation passed, but the dependency of ipc-shm-sample.ko is wrong.

And yes, I build it with yocto project.

 

Thanks,

Zhantao

0 件の賞賛
返信