IPCF log error (failed to get buffer)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IPCF log error (failed to get buffer)

Jump to solution
6,073 Views
Abhiram_m_s
Contributor I

Hello,
I have been trying to solve the example project which was given in the IPCF 4.9.0 package. 
I was following the below steps,

Abhiram_m_s_0-1710994319940.pngAbhiram_m_s_0-1710994319940.png

The expected output has to be like

Abhiram_m_s_1-1710994371478.pngAbhiram_m_s_1-1710994371478.png

But i am getting an error as follows when i try to ping

Abhiram_m_s_2-1710994414997.pngAbhiram_m_s_2-1710994414997.png

 

Please let me know how to debug this error.

Note : I am using

  • IPCF 4.9.0
  • RTD 4.0.2
  • S32DS 3.5.3
  • Linux BSP 38
  • FreeRtos 4.0.2
0 Kudos
Reply
1 Solution
5,907 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @Abhiram_m_s

Thanks for the feedback.

  1. Firstly, you may have the toolchain prepared, according to the BSP38.0UM, you may download it to your host:

chenyin_h_0-1711702897200.pngchenyin_h_0-1711702897200.png

Unzip the toolchain to your specific path, for example, /home/test/toolchain

  1. Secondly, download and compile the kernel source, following 3.2.3 of BSPUM for the details, for example, the kernel source is put to the /home/test/kernel
  2. At last, compile the modules of IPCF4.9

git clone https://github.com/nxp-auto-linux/ipc-shm.git

git checkout SW32G_IPCF_4.9.0_D2310

make CROSS_COMPILE= /home/test/toolchain/arm-gnu-toolchain-11.3.rel1-x86_64-aarch64-none-linux-gnu/bin/aarch64-none-linux-gnu- PLATFORM_FLAVOR=s32g3 KERNELDIR=/home/test/kernel

Then the new *.ko files would be generated.

Copy them to the RFS of BSP38.0, insmod them as indicated from the IPCF manual.

Hope it helps.

 

Best Regards

Chenyin

View solution in original post

0 Kudos
Reply
13 Replies
5,813 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @Abhiram_m_s

Thanks for the feedback.

May I know from M core side, which project/application you are running during the test? IPCF_Example_S32G399A_M7_0 or others?

 

Best Regards

Chenyin

 

0 Kudos
Reply
5,771 Views
Abhiram_m_s
Contributor I

Hello @chenyin_h ,
The solution you provided worked when I ran IPCF_Example_multi_instance_S32G399A_M7 example. Thank you for your help.

0 Kudos
Reply
5,806 Views
Abhiram_m_s
Contributor I

Hi @chenyin_h ,
From m core side we have been using IPCF_FreeRTOS_S32G399A_M7_0 example.

0 Kudos
Reply
5,841 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @Abhiram_m_s

Thanks for the feedback, seems the kernel module does not match the kernel from your log. I have the following two options for your reference.

  1. From my last post, in step2, assuming you have built the kernel image. Then, put the newly built kernel image to the SD card instead of the default one, have a try with the new built modules with this new kernel.
  2. If the current kernel you used is the default one built from Yocto, you may not use the standalone kernel path during the module compiling, instead, you may set the kernel path to the yocto kernel build path, which may like: …/build_s32g274ardb2/tmp/work/s32g274ardb2-fsl-linux/linux-s32/5.15.119-r0/build, then rebuilt the new modules to have a try.

Hope it helps

 

Best Regards

Chenyin

0 Kudos
Reply
5,834 Views
Abhiram_m_s
Contributor I

Hello @chenyin_h ,
I followed the step 2 as u mentioned, ipc-shm-dev.ko file got inserted, but when i try to insert ipc-shm-sample_multi_instance.ko, i am getting the following error : 

Abhiram_m_s_0-1712038463797.pngAbhiram_m_s_0-1712038463797.png

Please let me know how to proceed.

0 Kudos
Reply
5,908 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @Abhiram_m_s

Thanks for the feedback.

  1. Firstly, you may have the toolchain prepared, according to the BSP38.0UM, you may download it to your host:

chenyin_h_0-1711702897200.pngchenyin_h_0-1711702897200.png

Unzip the toolchain to your specific path, for example, /home/test/toolchain

  1. Secondly, download and compile the kernel source, following 3.2.3 of BSPUM for the details, for example, the kernel source is put to the /home/test/kernel
  2. At last, compile the modules of IPCF4.9

git clone https://github.com/nxp-auto-linux/ipc-shm.git

git checkout SW32G_IPCF_4.9.0_D2310

make CROSS_COMPILE= /home/test/toolchain/arm-gnu-toolchain-11.3.rel1-x86_64-aarch64-none-linux-gnu/bin/aarch64-none-linux-gnu- PLATFORM_FLAVOR=s32g3 KERNELDIR=/home/test/kernel

Then the new *.ko files would be generated.

Copy them to the RFS of BSP38.0, insmod them as indicated from the IPCF manual.

Hope it helps.

 

Best Regards

Chenyin

0 Kudos
Reply
5,855 Views
Abhiram_m_s
Contributor I

Hi @chenyin_h ,
We used the toolchain GCC 11.3.0 as u mentioned above and we built the ipc-shm-dev.ko and ipc-shm-sample_multi_instance.ko.
When i insmod the ipc-shm-dev.ko, i am getting following error.

Abhiram_m_s_0-1711952746850.pngAbhiram_m_s_0-1711952746850.png

 

Please let us know how to proceed

You can see the .ko files being generated

Abhiram_m_s_1-1711952826099.pngAbhiram_m_s_1-1711952826099.png

 

0 Kudos
Reply
5,932 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @Abhiram_m_s

Thanks for the feedback.

I have the following input for your reference.

git clone https://github.com/nxp-auto-linux/ipc-shm.git

git checkout SW32G_IPCF_4.9.0_D2310

make CROSS_COMPILE=/TOOLCHAINPATH/arm-gnu-toolchain-11.3.rel1-x86_64-aarch64-none-linux-gnu/bin/aarch64-none-linux-gnu- PLATFORM_FLAVOR=s32g3 KERNELDIR=/KERNELPATH

Then the new *.ko files would be generated.

Hope it helps.

 

Best Regards

Chenyin

0 Kudos
Reply
5,929 Views
Abhiram_m_s
Contributor I
Hi,
We used BSP38 yocto build... And we are not sure where to find the following paths in the repo which we cloned (yocto BSP38).
TOOLCHAINPATH
KERNELPATH
Can you please let us know how to locate the toolchain and linux kernel?
0 Kudos
Reply
5,971 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @Abhiram_m_s

Thanks for the feedback, the most possible reason is that the version used under Linux is not correct, my suggestions are as follows:

  1. The RFS from BSP38.0 is correct for testing the IPCF4.9
  2. However, do not use the default *.ko files under /lib/modules/, since the code version is not compatible with the demo/example you were running.
  3. Instead, download the code from https://github.com/nxp-auto-linux/ipc-shm, checkout the IPCF4.9.0, then build out module files.(*.ko)
  4. Copy the newly built *.ko files to your RFS, insmod them, then continue your test to have a try.

Hope it helps.

 

Best Regards

Chenyin

0 Kudos
Reply
5,946 Views
Abhiram_m_s
Contributor I

Hello @chenyin_h ,

Since we are new to this, can you let us know hot to build the .ko files which was mention by you in point number 3. 

Thank you.

 

0 Kudos
Reply
6,010 Views
chenyin_h
NXP Employee
NXP Employee

Hello, @Abhiram_m_s

Thanks for the questions

May I know when you are preparing the test from Linux side, you were using the default module files from the RFS or compiled them yourselves?

If you were using the default one, then there may be issues,  you may have to build the corresponding modules from IPCF4.9 and then use it in your Linux side.

Hope it helps.

 

Best Regards

Chenyin

0 Kudos
Reply
6,008 Views
Abhiram_m_s
Contributor I

Hello,
We have also tried with our own rfs BSP 37.0 but we are getting the same error. Even with 38.0 we are getting the same error.
If we are trying to run m core side by side we are getting Reset error.
The error is as follows :

Abhiram_m_s_0-1711101054685.pngAbhiram_m_s_0-1711101054685.png

Please let me know how to proceed.

0 Kudos
Reply