IPCF_Example_S32G274A_M7_0 does not work

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IPCF_Example_S32G274A_M7_0 does not work

ソリューションへジャンプ
1,595件の閲覧回数
won0020
Contributor III

Hello,
I use S32G-VNO-GLDBOX ver. 47800 REV D1 with IPCF 4.9.0 D2310, RTD 4.0.2 D2306, Linux BSP 38.0.

I'm trying to run the example following the instructions from the description file, but I'm not able to get the expected result.

.intc_vector 0x34500400,
linker file settings:

won0020_0-1711460672531.pngwon0020_0-1711460672531.png,

ipcf peripheral settings:

won0020_1-1711460906465.pngwon0020_1-1711460906465.png,

loading the IPCF sample from u-boot console:

won0020_2-1711461012096.pngwon0020_2-1711461012096.png,

running sample app:

won0020_3-1711461194108.pngwon0020_3-1711461194108.png,

result:

won0020_4-1711461274560.pngwon0020_4-1711461274560.png.

Thank you in advance for your reply.

Best regards
won0020

 

 

 

0 件の賞賛
返信
1 解決策
1,588件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

This seems to be related to the following community thread:

Re: Issue with NXP S32G274A RDB2 -  IPCF - NXP Community

In which there is a conflict between IPCF versions (from IPCF example and IPCF under Linux). A solution was provided on the link above.

Hope it helps with this inquiry.

Please, let us know.

元の投稿で解決策を見る

2 返答(返信)
1,589件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

This seems to be related to the following community thread:

Re: Issue with NXP S32G274A RDB2 -  IPCF - NXP Community

In which there is a conflict between IPCF versions (from IPCF example and IPCF under Linux). A solution was provided on the link above.

Hope it helps with this inquiry.

Please, let us know.

1,573件の閲覧回数
won0020
Contributor III
Hi,
I reconfigured the entire S32DS example 4.9.0 according to 4.8.0 and now it works with BSP 38.0 and 39.0.
Thank you very much.
0 件の賞賛
返信