How to validate Reference Board S32G RDB2?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to validate Reference Board S32G RDB2?

2,742 次查看
JunmoKang
Contributor I

I wanna buy RDB2 and validate our Memory.

Can i receive SW or Test list for validation?

 

0 项奖励
回复
5 回复数

2,503 次查看
JunmoKang
Contributor I

Hi, Daniel.

actually, we bought RDB, but I can't found some validation procedure or test procedure.

Can you help me for validation this RDB and our memory component?

 

Best regards,

Junmo.

0 项奖励
回复

2,472 次查看
JunmoKang
Contributor I

I think AN12848 describes only Calibration and Training, isn't it?

0 项奖励
回复

2,708 次查看
JunmoKang
Contributor I

Thank you for your detail explanation.

Is there any SI or Logic measurement in validation process? Can we get validation through Test report with only test and log file?

I can't find any detail test requirement.

I'd greatly appreciate any help you can offer.

0 项奖励
回复

2,682 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

An in-depth explanation of the DDR validation is provided under AN12848, which can be accessed through the S32G2 product page (link: S32G2 Safe and Secure Vehicle Network Processor | NXP Semiconductors). In here, usage and tests are described, could be better than trying to explain all the tests.

As for SI, we see that it provides an eye-diagram for each DQ line, don't know if this is what you are looking for.

Please, let us know.

0 项奖励
回复

2,728 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

S32G SW packages are provided under the "Automotive Software Package Manager", available under the S32G2 product page (link: S32G2 Safe and Secure Vehicle Network Processor | NXP Semiconductors) inside the "Software" section.

Once you select the option, you will be redirected to another page where you can select the platform and either choose one of the available bundles or create your own. Since this will require approval from the NXP team, your bundle will be available to download once this happens. This can be delayed from 1 to 2 days.

For DDR validation, there are some tests already available inside Config Tools (bundled inside S32 Design Studio), which is used to verify the DDR parameters. For this, you should require both the "Real-Time Drivers (RTD)" and the "S32G development package". The latter should be provided inside S32 Design Studio, it just needs to be installed. More information on regards of the package installation is provided under the following link:

S32DS Extensions & Updates: Explanation and How To... - NXP Community

Please, let us know.

0 项奖励
回复