How to use LLCE flexray and LLCE LIN A core

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use LLCE flexray and LLCE LIN A core

Jump to solution
1,630 Views
StanleyShen
Contributor IV

Since the LLCE supports 4 LINs and 1 Fleyray, could you tell me how to use them in A core 

Thank you.

0 Kudos
Reply
1 Solution
1,566 Views
nxf92355
NXP Employee
NXP Employee

Hi Stanley Shen

 

Hope you are doing well

Current Linux BSP releases do not include support for the LLCE LIN and LLCE FlexRay protocols. we suggest you go with M7. as of now there are no plans to add them in bsp.

 

Regards ,

Tushar

View solution in original post

0 Kudos
Reply
1 Reply
1,567 Views
nxf92355
NXP Employee
NXP Employee

Hi Stanley Shen

 

Hope you are doing well

Current Linux BSP releases do not include support for the LLCE LIN and LLCE FlexRay protocols. we suggest you go with M7. as of now there are no plans to add them in bsp.

 

Regards ,

Tushar

0 Kudos
Reply