How to use LLCE flexray and LLCE LIN A core

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to use LLCE flexray and LLCE LIN A core

ソリューションへジャンプ
1,627件の閲覧回数
StanleyShen
Contributor IV

Since the LLCE supports 4 LINs and 1 Fleyray, could you tell me how to use them in A core 

Thank you.

0 件の賞賛
返信
1 解決策
1,563件の閲覧回数
nxf92355
NXP Employee
NXP Employee

Hi Stanley Shen

 

Hope you are doing well

Current Linux BSP releases do not include support for the LLCE LIN and LLCE FlexRay protocols. we suggest you go with M7. as of now there are no plans to add them in bsp.

 

Regards ,

Tushar

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,564件の閲覧回数
nxf92355
NXP Employee
NXP Employee

Hi Stanley Shen

 

Hope you are doing well

Current Linux BSP releases do not include support for the LLCE LIN and LLCE FlexRay protocols. we suggest you go with M7. as of now there are no plans to add them in bsp.

 

Regards ,

Tushar

0 件の賞賛
返信