How to include s32g_pfe_class.fw and g32g_pfw_uilt.fw in /lib/firmware

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to include s32g_pfe_class.fw and g32g_pfw_uilt.fw in /lib/firmware

ソリューションへジャンプ
3,063件の閲覧回数
Inchul
Contributor II

Hi,

 

I am using S32G-PROCEVB-S and S32GRV-PLATEVB in stacked mode. I made the SDCARD image  by using Yocto. But I could not found s32g_pfe_class.fw and s32g_pfe_util.fw in the /lib/firmware folder on target board system. I cannot active pfe1 and pfe2 network interface now. How can I include s32g_pfe_class.fw and s32g_pfe_util.fw into SDCARD imgae?

 

When I used the pre-built BSP 29.0 SDCARD image, I could see s32g_pfe_class.fw and s32g_pfe_util.fw in the /lib/firmware and boot partition.

 

And I could not found modules as the following.

./lib/modules/5.4.69-rt39+ge2e9a4afb7c5/kernel/drivers/net/ethernet/nxp/pfe/pfeng-2.0.ko
./lib/modules/5.4.69-rt39+ge2e9a4afb7c5/kernel/drivers/net/ethernet/nxp/pfe/pfeng-1.1.ko

 

For your reference, I used repository as the following.

https://source.codeaurora.org/external/autobsps32/auto_yocto_bsp -b hotfix/bsp29.0.hf1 

 

Thank you and best regards.

 

0 件の賞賛
1 解決策
3,042件の閲覧回数
bpe
NXP Employee
NXP Employee

This is a duplicate. See this thread for suggestions. Please avoid making duplicate posts in future.

Best Regards,
Platon

 

 

元の投稿で解決策を見る

1 返信
3,043件の閲覧回数
bpe
NXP Employee
NXP Employee

This is a duplicate. See this thread for suggestions. Please avoid making duplicate posts in future.

Best Regards,
Platon