How to include s32g_pfe_class.fw and g32g_pfw_uilt.fw in /lib/firmware

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to include s32g_pfe_class.fw and g32g_pfw_uilt.fw in /lib/firmware

跳至解决方案
3,062 次查看
Inchul
Contributor II

Hi,

 

I am using S32G-PROCEVB-S and S32GRV-PLATEVB in stacked mode. I made the SDCARD image  by using Yocto. But I could not found s32g_pfe_class.fw and s32g_pfe_util.fw in the /lib/firmware folder on target board system. I cannot active pfe1 and pfe2 network interface now. How can I include s32g_pfe_class.fw and s32g_pfe_util.fw into SDCARD imgae?

 

When I used the pre-built BSP 29.0 SDCARD image, I could see s32g_pfe_class.fw and s32g_pfe_util.fw in the /lib/firmware and boot partition.

 

And I could not found modules as the following.

./lib/modules/5.4.69-rt39+ge2e9a4afb7c5/kernel/drivers/net/ethernet/nxp/pfe/pfeng-2.0.ko
./lib/modules/5.4.69-rt39+ge2e9a4afb7c5/kernel/drivers/net/ethernet/nxp/pfe/pfeng-1.1.ko

 

For your reference, I used repository as the following.

https://source.codeaurora.org/external/autobsps32/auto_yocto_bsp -b hotfix/bsp29.0.hf1 

 

Thank you and best regards.

 

0 项奖励
1 解答
3,041 次查看
bpe
NXP Employee
NXP Employee

This is a duplicate. See this thread for suggestions. Please avoid making duplicate posts in future.

Best Regards,
Platon

 

 

在原帖中查看解决方案

1 回复
3,042 次查看
bpe
NXP Employee
NXP Employee

This is a duplicate. See this thread for suggestions. Please avoid making duplicate posts in future.

Best Regards,
Platon