How to download BSP30.0 yocto repo after the migrate codeaurora to github

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to download BSP30.0 yocto repo after the migrate codeaurora to github

2,057 Views
StanleyShen
Contributor IV

Hi there

It seems that recently NXP repos moved from codeaurora to github.

How can I download the BSP33.0 from github.

After I am initialize the repo like blow

 

repo init -u https://github.com/nxp-auto-linux/auto_yocto_bsp -b release/bsp30.0 --repo-url='https://mirrors.tuna.tsinghua.edu.cn/git/git-repo/'
Downloading Repo source from https://mirrors.tuna.tsinghua.edu.cn/git/git-repo/
remote: Enumerating objects: 4460, done.
remote: Counting objects: 100% (4460/4460), done.
remote: Compressing objects: 100% (2121/2121), done.
remote: Total 8034 (delta 3974), reused 2339 (delta 2339), pack-reused 3574
Receiving objects: 100% (8034/8034), 3.75 MiB | 13.15 MiB/s, done.
Resolving deltas: 100% (5167/5167), done.

Your identity is: Your Name <you@example.com>
If you want to change this, please re-run 'repo init' with --config-name

repo has been initialized in /home/grce/fsl-auto-yocto-bsp

 

and sync it like this

 

repo sync

 

It seems like they still  access to  source.codeaurora.org

 

$ repo sync
remote: Enumerating objects: 21, done.
remote: Counting objects: 100% (21/21), done.
remote: Compressing objects: 100% (4/4), done.
remote: Total 15 (delta 11), reused 15 (delta 11), pack-reused 0
Unpacking objects: 100% (15/15), done.
Fetching:  0% (0/9) warming upb'  % Total    % Received % Xferd  Average Speed   Time    Time     Time  Current\n                                 Dload  Upload   Total   Spent    Left  Speed\n\r  0     0    0     0    0     0      0      0 --:--:-- --:--:-- --:--:--     0\r  0     0    0     0    0     0      0      0 --:--:-- --:--:-- --:--:--     0curl: (6) Could not resolve host: source.codeaurora.org\n'

fatal: unable to access 'https://source.codeaurora.org/external/autobsps32/meta-alb/': Could not resolve host: source.codeaurora.org

meta-alb:
fatal: unable to access 'https://source.codeaurora.org/external/autobsps32/meta-alb/': Could not resolve host: source.codeaurora.org
meta-alb: sleeping 4.0 seconds before retrying
fatal: unable to access 'https://source.codeaurora.org/external/autobsps32/meta-alb/': Could not resolve host: source.codeaurora.org

meta-alb:
fatal: unable to access 'https://source.codeaurora.org/external/autobsps32/meta-alb/': Could not resolve host: source.codeaurora.org
error: Cannot fetch meta-alb from https://source.codeaurora.org/external/autobsps32/meta-alb

 

But why?

Have you not completed the migration yet?

Is it still not possible to correctly download the yocto project code even after source.codeaurora.org is no longer accessible?

Do you have any alternative solutions to download the BSP30.0 source code?

Thank you!

3 Replies

2,045 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Please take a look in the following Post that also apply to S32G devices

Linux source code migration (CAF -> Github) - NXP Community

Regards

0 Kudos
Reply

1,832 Views
Gerry15
Contributor III

Hey,

 

I wanted to build Yocto on the S32G and used the S32G_LinuxBSP_33.0_User_Manual to do so. As already discussed in this thread, the following line will not work anymore:

 

 

repo init -u https://source.codeaurora.org/external/autobsps32/auto_yocto_bsp -b release/bsp33.0

 

 

 Could you give a concrete example for this case, how I can find the correct repo?

 

"repo init -u https://github.com/nxp-auto-linux/auto_yocto_bsp.git -b release/bsp33.0" is also not working as it still somehow uses codeaurora:

Update

  • bsp36.0 is the only active release branch, therefore using this branch does not use codeaurora anymore

 

Kind Regards

0 Kudos
Reply

1,804 Views
StanleyShen
Contributor IV

@Gerry15 

I am sorry, I am not the NXP employee, so my answer is for reference only.

Since codeaurora has been closed, I strongly recommend that you consider compiling BSP35.0(or above) directly instead of downloading and compiling BSP30.0 on Github.

here is the cmd for BSP35.0 download

repo init -u https://github.com/nxp-auto-linux/auto_yocto_bsp -b release/bsp35.0

 after that, pls following the BSP30.0 menual to compile it.

Otherwise 

If you must compile BSP30.0, modifying the content of the configuration file in the. repo folder may be a necessary

Such as, modify 

https://source.codeaurora.org/external/qoriq/qoriq-components/meta-qoriq/

to https://github.com/nxp-qoriq/meta-qoriq