about the efuse read limitation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

about the efuse read limitation

Jump to solution
651 Views
brian_w
Contributor III

Hi,

 In the G2 rm, it's said the read limitation is 20m times per bit.

brian_w_0-1684756923339.png

 After every standby mode exist, there will be a destructive reset and the efuse need to be read again. If G2 swtiches between standby mode and fast boot mode frequently, after some time, the efuse will have problem?

 How should I avoid to damage the efuse?

0 Kudos
Reply
1 Solution
638 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

If the accumulative reads to a specific bit surpasses 2 million reads, we cannot longer confirm the correct functioning on regards of the read operation under the eFuses (which should be around 550 reads per day under a 10-year lifespan, under a single bit).

Since this is part of platform, there is no plan or document on how to avoid damage to the eFuse. One possibility is to have a copy of the fuses on an external EEPROM, for redundancy.

Please, let us know.

View solution in original post

0 Kudos
Reply
1 Reply
639 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

If the accumulative reads to a specific bit surpasses 2 million reads, we cannot longer confirm the correct functioning on regards of the read operation under the eFuses (which should be around 550 reads per day under a 10-year lifespan, under a single bit).

Since this is part of platform, there is no plan or document on how to avoid damage to the eFuse. One possibility is to have a copy of the fuses on an external EEPROM, for redundancy.

Please, let us know.

0 Kudos
Reply