GMAC Fixed-link mode TX OK, RX NG

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GMAC Fixed-link mode TX OK, RX NG

ソリューションへジャンプ
2,945件の閲覧回数
StanleyShen
Contributor IV
 
Hi there.

We had a problem using PFE for MAC2MAC connection before, but we haven't received an answer.

RMII & Fixed-link under PFE TX OK but RX NG - NXP Community

So we have now used GMAC for testing.

The device tree has been modified as follows, but it has been found that the problem is the same. Can you please explain the reason to me? Are there any issues with NXP's MAC2MAC support?

 

diff --git a/arch/arm64/boot/dts/freescale/s32gxxxa-rdb.dtsi b/arch/arm64/boot/dts/freescale/s32gxxxa-rdb.dtsi
index e1fbd28bb..98544ff9c 100644
--- a/arch/arm64/boot/dts/freescale/s32gxxxa-rdb.dtsi
+++ b/arch/arm64/boot/dts/freescale/s32gxxxa-rdb.dtsi
@@ -23,15 +23,26 @@
        status = "okay";
        pinctrl-names = "default";
        pinctrl-0 = <&gmac0rgmiia_pins>, <&gmac0mdioa_pins>;
-       phy-handle = <&gmac_mdio_a_phy1>;
-       phy-mode = "rgmii-id";
+//     phy-handle = <&gmac_mdio_a_phy1>;
+       phy-mode = "rgmii";
+        fixed-link {
+                speed = <10>;
+                full-duplex;
+        };
 };

 

0 件の賞賛
返信
1 解決策
2,871件の閲覧回数
MayanksPatel
NXP Employee
NXP Employee

Hi @StanleyShen,

The same suggestion for GMAC was previously provided for PFE.

you can use a GPIO signal, which is controlled in Linux, to enable the 5G module.

So the solution for that is to bring up the 5G module as early as possible before initializing the related clock.

 

Thanks,

Mayank S Patel

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,822件の閲覧回数
StanleyShen
Contributor IV

Hi @MayanksPatel 

Thank you for you replay.

Previously, we also found this situation and resolved it using the same method.

Thank you again

 

0 件の賞賛
返信
2,898件の閲覧回数
MayanksPatel
NXP Employee
NXP Employee

Hi @StanleyShen,

Sorry for the delay.

I have created a ticket with the internal team for the same and I will get back to you on this.

Thank you for your patience.

 

Thanks,

Mayank S Patel

0 件の賞賛
返信
2,872件の閲覧回数
MayanksPatel
NXP Employee
NXP Employee

Hi @StanleyShen,

The same suggestion for GMAC was previously provided for PFE.

you can use a GPIO signal, which is controlled in Linux, to enable the 5G module.

So the solution for that is to bring up the 5G module as early as possible before initializing the related clock.

 

Thanks,

Mayank S Patel

0 件の賞賛
返信