S32G3 PFE Slave configuration query

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32G3 PFE Slave configuration query

1,678 次查看
s153022
Contributor III

I have successfully built the NXP Auto Linux BSP 35.0 by cloning the repository from https://github.com/nxp-auto-linux/auto_yocto_bsp, using the branch release/bsp35.0.

The build process has resulted in the creation of the dtb with PFE configured as master.

However, we require the PFE slave.

I found the slave dtsi in the kernel source at `arch/arm64/boot/dts/freescale/s32g-pfe-slave.dtsi` 

 

Is there any tidy way  to configure the yocto  build to generate the PFE slave rather than manually updating the dtb?

 

we have both the `pfe-slave and pfe` in yocto configuration (local.conf)

 

Also, is it possible to have both master and slave configuration simultaneously?

 

Thank you for your help and consideration.

Best regards

Sami

标记 (2)
0 项奖励
回复
1 回复

1,627 次查看
MayanksPatel
NXP Employee
NXP Employee

Hi @s153022,

Thank you for reaching out to us.

For configuring, Master and slave interface you should configure the flexible router, and with the help of the libfci library, you can create instance of slave and master.

First, you need to configure the Master interface and once communication is up, you need to load the slave driver.

Please reference is provided in the document "PFE_S32G_A53_LNX_UserManual.pdf Section 2.5 Master-Slave instances".

 

Hope this helps.

 

Thanks,

Mayank S Patel

 

0 项奖励
回复