Flash Read Alignment Issue - Data Reads from 2n Instead of 2n+1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flash Read Alignment Issue - Data Reads from 2n Instead of 2n+1

ソリューションへジャンプ
1,102件の閲覧回数
zyz
Contributor III
Recently, when using the S32G274 M7 core to read data from flash, I encountered a forced alignment issue. When attempting to read data starting from an address 2n+1, the returned data starts from address 2n. However, reading from address 2n does not have this problem. We are bypassing FEE and directly using the FLS driver to operate the flash. The MCAL version is: SWS32G_RTD_4.4_4.0.2.
 
Who can help me, thank you.
0 件の賞賛
返信
1 解決策
1,012件の閲覧回数
zyz
Contributor III
Hi carlos_o,
Thank you for your support. I have already solved the problem on my side. This 2-byte alignment issue is caused by the inherent characteristics of FLASH and is not related to the software.

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
1,081件の閲覧回数
carlos_o
NXP TechSupport
NXP TechSupport

Hi @zyz,

Are you using a custom board? if not is it an RDB or EVB? 

If you are using a custom board, which model of QSPI are you using? 

The problem is when you are doing the bypass of the FEE driver and using directly the FLS? or this is a workaround? 

 

 

0 件の賞賛
返信
1,071件の閲覧回数
zyz
Contributor III

Hello carlos_o,

Yes, I am using our custom board with QSPI DDR mode. The flash model is MX25UW51245G.
 
I discovered this issue when directly using FLS.
0 件の賞賛
返信
1,039件の閲覧回数
carlos_o
NXP TechSupport
NXP TechSupport

Hi @zyz 

I recommend try first with the IP functions instead of MCAL, you can see how it works at the Spi_Ip_Transfer example. Let me know if the issue persists. 

0 件の賞賛
返信
1,013件の閲覧回数
zyz
Contributor III
Hi carlos_o,
Thank you for your support. I have already solved the problem on my side. This 2-byte alignment issue is caused by the inherent characteristics of FLASH and is not related to the software.
0 件の賞賛
返信
1,000件の閲覧回数
carlos_o
NXP TechSupport
NXP TechSupport

Hi @zyz

great to hear that. Let us know if there is anything we can do to help.

0 件の賞賛
返信